How to change the logical output voltage of FRDMKW36?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to change the logical output voltage of FRDMKW36?

Jump to solution
1,435 Views
Enjoy
Contributor II

Hi there:

I want to drive a external ADC by FRDMKW36, while when I set one GPIO of MKW36 to 1, the output voltage is only about 1.8v and too low to enable the ADC. So can the logical output volatage of GPIO rise to about 3v in FRDMKW36?

May somebody help me?

Thanks.

Labels (1)
0 Kudos
Reply
1 Solution
1,428 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. Could you please check this Application Note: DC-DC Power Management?

The FRDM-KW36 can be configured to use any of the DCDC converter operating modes. The board is configured in Buck (Auto-Start) by default.

Also, please refer to FRDM-KW36 Freedom Development Board User's Guide. (Section 3.3: Power management).

Hope this helps.

 

Regards,

Ricardo

View solution in original post

2 Replies
1,429 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. Could you please check this Application Note: DC-DC Power Management?

The FRDM-KW36 can be configured to use any of the DCDC converter operating modes. The board is configured in Buck (Auto-Start) by default.

Also, please refer to FRDM-KW36 Freedom Development Board User's Guide. (Section 3.3: Power management).

Hope this helps.

 

Regards,

Ricardo

1,424 Views
Enjoy
Contributor II
Thank you so much and the problem has been solved.
0 Kudos
Reply