How to Plot XY graph with eGUI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Plot XY graph with eGUI

ソリューションへジャンプ
3,964件の閲覧回数
lordtheo
Contributor I

Good Morning everyone

My Name is Theo. I have the following question

I am trying to plot XY graph using eGUI and I don't know how to do it.

My understanding is that the function D4D_GraphAddTracesData(pObj, pValues) will only plot pValues from what I tried.

What I would like is to plot XY. Let's say I have the following table

________________________________________________

X    0     5     11    18    20

Y    0     28   56    14    5

________________________________________________

How do I plot so that on the X-Axis and on the Y-Axis, it will show the corresponding value ?

Is it possible?

Any help will be really appreciate.

Best Regards,

--

Theo.

ラベル(1)
0 件の賞賛
返信
1 解決策
3,796件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

Find attached an example to GRAPH plotting a sinusoidal function.

Luis

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,795件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Yes, file is in the thread.

Luis

0 件の賞賛
返信
3,797件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

Find attached an example to GRAPH plotting a sinusoidal function.

Luis

0 件の賞賛
返信
3,795件の閲覧回数
lordtheo
Contributor I

Hi

I don't see any attached file. Could you re-send please?

Best Regards,

--

Theo.

0 件の賞賛
返信
3,795件の閲覧回数
bobpaddock
Senior Contributor IV

To see the attached file click on the subject line that started this thread so that the thread becomes full screen.

Also you must be logged in to download.

0 件の賞賛
返信