How to Plot XY graph with eGUI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to Plot XY graph with eGUI

Jump to solution
4,200 Views
lordtheo
Contributor I

Good Morning everyone

My Name is Theo. I have the following question

I am trying to plot XY graph using eGUI and I don't know how to do it.

My understanding is that the function D4D_GraphAddTracesData(pObj, pValues) will only plot pValues from what I tried.

What I would like is to plot XY. Let's say I have the following table

________________________________________________

X    0     5     11    18    20

Y    0     28   56    14    5

________________________________________________

How do I plot so that on the X-Axis and on the Y-Axis, it will show the corresponding value ?

Is it possible?

Any help will be really appreciate.

Best Regards,

--

Theo.

Labels (1)
0 Kudos
Reply
1 Solution
4,032 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

Find attached an example to GRAPH plotting a sinusoidal function.

Luis

View solution in original post

0 Kudos
Reply
4 Replies
4,031 Views
LuisCasado
NXP Employee
NXP Employee

Yes, file is in the thread.

Luis

0 Kudos
Reply
4,033 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

Find attached an example to GRAPH plotting a sinusoidal function.

Luis

0 Kudos
Reply
4,031 Views
lordtheo
Contributor I

Hi

I don't see any attached file. Could you re-send please?

Best Regards,

--

Theo.

0 Kudos
Reply
4,031 Views
bobpaddock
Senior Contributor III

To see the attached file click on the subject line that started this thread so that the thread becomes full screen.

Also you must be logged in to download.

0 Kudos
Reply