How to Plot XY graph with eGUI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to Plot XY graph with eGUI

跳至解决方案
3,954 次查看
lordtheo
Contributor I

Good Morning everyone

My Name is Theo. I have the following question

I am trying to plot XY graph using eGUI and I don't know how to do it.

My understanding is that the function D4D_GraphAddTracesData(pObj, pValues) will only plot pValues from what I tried.

What I would like is to plot XY. Let's say I have the following table

________________________________________________

X    0     5     11    18    20

Y    0     28   56    14    5

________________________________________________

How do I plot so that on the X-Axis and on the Y-Axis, it will show the corresponding value ?

Is it possible?

Any help will be really appreciate.

Best Regards,

--

Theo.

标签 (1)
0 项奖励
回复
1 解答
3,786 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

Find attached an example to GRAPH plotting a sinusoidal function.

Luis

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,785 次查看
LuisCasado
NXP Employee
NXP Employee

Yes, file is in the thread.

Luis

0 项奖励
回复
3,787 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

Find attached an example to GRAPH plotting a sinusoidal function.

Luis

0 项奖励
回复
3,785 次查看
lordtheo
Contributor I

Hi

I don't see any attached file. Could you re-send please?

Best Regards,

--

Theo.

0 项奖励
回复
3,785 次查看
bobpaddock
Senior Contributor IV

To see the attached file click on the subject line that started this thread so that the thread becomes full screen.

Also you must be logged in to download.

0 项奖励
回复