How to Create ".SREC" Output file in Codewarriors 10.3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to Create ".SREC" Output file in Codewarriors 10.3

跳至解决方案
5,250 次查看
ashokra
Contributor II

Hi Iam new to Freescale and working with Kinetis Controller. I brought Freedom Development Kit and i installed code warriors v10.3.

I downloaded FRDM-KL25Z Quick Start Package In that i could see some precompiled example (i.e "*****.srec" output files ) but I am not able to create ".srec" output file with codewarriors. i just want to develop simple LED blinking project can anyone help me?

标签 (1)
标记 (1)
1 解答
1,905 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

- How to generate SREC (or S19) file: S-Record Generation with gcc for ARM/Kinetis | MCU on Eclipse

- LED's with the Freedom board: Tutorial: Enlightning the Freedom KL25Z Board | MCU on Eclipse

- Other things for the Freedom board: KL25Z Freedom Board | MCU on Eclipse

Hope this helps.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,905 次查看
ashokra
Contributor II

Thank you!  Erich , its very useful.... :-)

0 项奖励
回复
1,905 次查看
SriViswatej_R_v
Contributor I

Hello ,

I'm new to free scale FRDM KL25 board.

I installed code warrior 10.5.

I downloaded the sample code.

I have seen the Quickstart package.

The pre-compiled code works well in the board.

But i'm unable to dump anything in the board. I want to dump the sample code in to it.

Please tell me the procedure to dump the coding into the board.

If possible please give me the link for reference.

Thank you.

0 项奖励
回复
1,906 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

- How to generate SREC (or S19) file: S-Record Generation with gcc for ARM/Kinetis | MCU on Eclipse

- LED's with the Freedom board: Tutorial: Enlightning the Freedom KL25Z Board | MCU on Eclipse

- Other things for the Freedom board: KL25Z Freedom Board | MCU on Eclipse

Hope this helps.

0 项奖励
回复