How to Create ".SREC" Output file in Codewarriors 10.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to Create ".SREC" Output file in Codewarriors 10.3

Jump to solution
6,142 Views
ashokra
Contributor II

Hi Iam new to Freescale and working with Kinetis Controller. I brought Freedom Development Kit and i installed code warriors v10.3.

I downloaded FRDM-KL25Z Quick Start Package In that i could see some precompiled example (i.e "*****.srec" output files ) but I am not able to create ".srec" output file with codewarriors. i just want to develop simple LED blinking project can anyone help me?

Labels (1)
Tags (1)
1 Solution
2,797 Views
BlackNight
NXP Employee
NXP Employee

Hello,

- How to generate SREC (or S19) file: S-Record Generation with gcc for ARM/Kinetis | MCU on Eclipse

- LED's with the Freedom board: Tutorial: Enlightning the Freedom KL25Z Board | MCU on Eclipse

- Other things for the Freedom board: KL25Z Freedom Board | MCU on Eclipse

Hope this helps.

View solution in original post

0 Kudos
Reply
3 Replies
2,797 Views
ashokra
Contributor II

Thank you!  Erich , its very useful.... :-)

0 Kudos
Reply
2,797 Views
SriViswatej_R_v
Contributor I

Hello ,

I'm new to free scale FRDM KL25 board.

I installed code warrior 10.5.

I downloaded the sample code.

I have seen the Quickstart package.

The pre-compiled code works well in the board.

But i'm unable to dump anything in the board. I want to dump the sample code in to it.

Please tell me the procedure to dump the coding into the board.

If possible please give me the link for reference.

Thank you.

0 Kudos
Reply
2,798 Views
BlackNight
NXP Employee
NXP Employee

Hello,

- How to generate SREC (or S19) file: S-Record Generation with gcc for ARM/Kinetis | MCU on Eclipse

- LED's with the Freedom board: Tutorial: Enlightning the Freedom KL25Z Board | MCU on Eclipse

- Other things for the Freedom board: KL25Z Freedom Board | MCU on Eclipse

Hope this helps.

0 Kudos
Reply