How "tower_bootloader” downloads into the chip?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How "tower_bootloader” downloads into the chip?

1,095 Views
wangb
Contributor II

How "tower_bootloader” downloads into the chip?Can I go through the serial port(uart)?Is there anything I can refer to?

0 Kudos
Reply
1 Reply

1,087 Views
nxf58904
NXP Employee
NXP Employee

Hi,

"tower_bootloader " means it is bootloader for tower board.And you can use IDE download it to chip via opensda or debugger.

 

Jianyu: 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply