Hi Pedro,
Thanks for your reply; I gave the case for a single ADC as I thought this would be simpler to explain however the full story is that we need to use the PDB to achieve simultaneous sampling of two ADC modules.
Explanation:
We have 4 signals
Signal_X - output from phase discriminator frequency range 2Hz to 44Hz
Signal_Y - output from phase discriminator frequency range 2Hz to 44Hz
I_Mon - coil current DC
+12V - supply voltage DC
The X,Y signals are converted into their polar form post ADC and Filtering so that phase angle and magnitude can be calculated, so as you can see we need excellent phase coherence between the sampled X&Y signals. Using the PDB to pre-trigger the ADC's gives us this. The results are excellent. The maximum sample rate is 2.8KHz
I need to measure the X and Y signals differentially as this gives use better noise immunity, however we only need to sample the other two signals single endedly. I would arrange the inputs as follows:-
X_input, I_mon -> ADC0
Y_input, +12v_mon ->ADC1
Taking ADC0 it is required that X_input, I_mon be sampled sequentially starting back at X_input in time for the next pre trigger from the PDB. The only constraint is that both the X_input and the I_mon input must be sampled within ~355us and that both X_input and Y_input must be sampled simultaneously.
So, from what you say I would be able to reconfigure the module/channels between each conversion?
As I understand it from the users manual, if I set the initial configuration to sample the differential channel when the pre trigger is received and then from within the ADC ISR write to SC1[ADCH] the next channel to be sampled, this would start the conversion on the selected channel straight away? I could then reconfigure the channel when I received the next ADC interrupt so that it is now sampling the differential input? However, as I understand it writing to SC1 starts the next conversion which is not what I want. The differential input must always be synchronised to the PDB. Can you advise
Thanks