How To Read Laptop's Touchpad Movement From KL25Z Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How To Read Laptop's Touchpad Movement From KL25Z Board

1,484 Views
ElectroDesi9n
Contributor II

Hi everyone,

 

I want to do a project with FRDM-KL25Z board and I was wondering is it possible to read my laptop's touchpad data from the board? Like making the touchpad data as input and the board will do a task if I swipe left, let's say.

If it is possible to do so, I would appreciate your full explaination of requirements and steps.

 

FRDM-KL25Z

0 Kudos
Reply
1 Reply

1,458 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

First of all, I suppose that you want to use PC to read the Touch pad movement on FRDM-KL25Z, the touchpad is connected to FRDM-KL25 instead of PC.

The KL25 has USB port, the PC USB can function as a host of HID class, the USB of FRDM-KL25 can function as device of HID class and send position of the touchpad in fixed cycle time.

Pls download SDK package of FRDM-KL25Z from the link:

https://mcuxpresso.nxp.com/en

On the PC side software, you can use C# or Python to develop the code, we do not support the firmware on PC side.

Hope it can help you

BR

XiangJun Rong