Hints how to use FNET TCP/IP stack on Kinetis K60DM256ZVLL10

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hints how to use FNET TCP/IP stack on Kinetis K60DM256ZVLL10

4,060 次查看
lucaognibene
Contributor II

Hello everybody!

I'm new in the community and I recently started to develop on this family of microcontrollers (Kinetis).

I need to implement a TCP/IP stack  on my system based on the K60DM256ZVLL10, so got the idea of using the promising and well-done FNET implementation (to avoid MQX which is too heavy for my purposes).

Since I read that FNET supports specifically the MK60N512 (TWR-K60N512 board) and apparently no other in the family, I'd like to know if it's possible (the main difference between my microcontroller and the MK60N512 is the amount of flash memory, right?)

If the answer is positive, which kind of actions do I have to do for reaching my aim?

Any special configuration/whatsoever?

Important thing to say that I need just basic things like TCP client/server and DHCP (no HTTP, SMTP, etc).

I planned to cut down FNET implementation.

In my board I use the same PHY chipset mounted on Tower K60 board (KSZ8041NL - not NE2000 register compatible AFAIK).

Let me know any hints and suggestions.

Kind regards,

   Luca O.

标签 (1)
标记 (4)
4 回复数

2,994 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Luca,

The major difference between K60DM256ZVLL10 with MK60N512 (TWR-K60N512 board) is Flash size and package (pin number). K60DM256ZVLL10 supports Ethernet RMII mode.

Both chips are based on Kinetis 100MHz silicon 1.x platform, there with same module registers definitions.

The FNET software doesn't not need be modified, which need to check the image size to match with 256KB flash size.

Wish it helps.

B.R.

Ma Hui

2,994 次查看
lucaognibene
Contributor II

Thanks a lot for the kind answer and for details.

I'm working on this project with a colleague, and effectively yesterday we managed to compile and run the stack on our board which uses the K60DM256 and the same Ethernet PHY chipset used on the Tower development board.

Due to the modular nature of the stack (thanks Andrey for fine config file) we "cut it down" for our purposes, removing telnet and HTTP, and its final size is really suitable for flash memory size (around 32kB).

Since we are using Processor Expert we needed to change a few parameters: I'll explain better what we did in next message.

We still have to understand what FatFS file system is for inside the stack.

Cheers!

   Luca O.

0 项奖励
回复

2,994 次查看
mjbcswitzerland
Specialist V

Luca

Also check out the uTasker project since it includes K60, K61, K70 support with a low-memory utilisation TCP/IP stack (IPv4/v6) which allows high-speed industrial-proven client/server operations (and of course DHCP). It is a complete project (not just stack) with low footprint OS, TCP/IP (various services such as FTP client and server, web server, TELNET, etc.), USB device, FAT and many drivers and other services.

It has a real-time Kinetis simulator which allows TCP/IP projects to be developed, run, debugged and tested on the PC (using VisualStudio) as well as containing GCC, CW10.x, Keil, IAR and Rowely Crossworks builds.

You can get an overview at http://www.utasker.com/kinetis.html

and see some videos of it operating on the Kinetis at:

- FTP_Client.wmv - YouTube

Kin_IPv6_1.wmv - YouTube

Regards

Mark

0 项奖励
回复

2,994 次查看
lucaognibene
Contributor II

Hello Mark!

Thanks for the suggestion.

Anyway we managed to put the FNET stack onto our microcontroller system (since the stack is the main thing we need), but we know another option to use in future projects.

Cheers,

   Luca O.

0 项奖励
回复