High Speed RNDIS and CDC composite (?)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

High Speed RNDIS and CDC composite (?)

1,200件の閲覧回数
mjbcswitzerland
Specialist V

Hi All

I am wondering whether anyone has used RNDIS + CDC composite on a K61 or K70's HS USB interface?

The issue that I have is that I can do this on any FS USB interface since they have 16 endpoints but the K61/K70's HS USB has just 4 and this configuration essentilly needs 5:

- Endpoint 0 - control

- Endpoint 1 - RNDIS bulk IN/OUT

- Endpoint 2 - RNDIS interrupt

- Endpoint 3 - CDC bulk IN/OUT

- Endpoint 4 - CDC interrupt

In fact the CDC interrupt endpoint is not used in practice but I don't know whether there is any way to configure so that it is not needed to satisfy the host or whether there is some other trick to get around this.

Any ideas (without having to move to K66 with 8 HS endpoints)???

Regards

Mark

ラベル(1)
0 件の賞賛
返信
0 返答(返信)