Help with Flexbus example on TWR-K53N512

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help with Flexbus example on TWR-K53N512

5,898件の閲覧回数
psantos
Contributor I

Hi All,

I've been attempting to attach a 16-bit parallel TFT display to my TWR-K53N512 TWR board via the Flexbus and I've been having issues. First with my D/C line not getting set and cleared correctly; and now no activity on my AD[0]-[15] lines. I was hoping someone can point me in the right direction.

Some background notes:

  • I'm heavily using the application note "Using FlexBus Interface for Kinetis Microcontrollers" as a reference(pg 14 LCD).  Since this app note uses the K60, I've had to do some pin remapping for the k53.
  • The display I'm using is a cfaf240320k024tts TFT Display, It pretty accurately functions the same as the one in the app note.
  • I'm using a USBee AX logic analyzer to probe lines
  • I've attached all relevant links at the end of the post
  • I'm using KDS v3.0
  • Since i'm using the TWR-K53N512 and KDS, I had to download The MK53DN512 SDK from mcuxpresso SDK Builder for register includes(Specifically #include <MK53D10.h>)
  • I've attached my code below
  • I haven't posted to the NXP fourms often so please feel free to let me know if I need to move the post to the appropriate area 

Questions:

  1. I can't get my D/C line(FB_ad[16]) to toggle when i'm trying to send a command vs data.
    1. Oddly enough after poking around I found a signal that looks like what it is supposed to be but it is on FB_AD[18] instead of FB_AD[16]. Why is this not on 16 or what is this signal?
  2. In general does anything look wrong in the code? I originally only had the issue with my D/C line, but now I can't get any activity on my AD[0]-[15] lines. I've attempted to revert back to a working version but I still can't get anything from them except a few 1-0 or 0-1 random transitions.
  3. How does setting CMSR0[BAM] define the block size?
    • In the example "Using FlexBus Interface for Kinetis Microcontrollers", They state that:
      • Setting the base address mask to 1 (CSMR0[BAM]) = 1) means that the block size for the CS is 2^n (n = number of bits in CSMR[BAM] + 16) must be 128 KB. This means address 0x60000000 to 0x6001FFFF can be accessed by the CS. Therefore address 0x6000000 (FB_AD16 is low) can be used to access the index register of the SSD1289, and address 0x60010000 (FB_AD16 is high) can be used to access the data buffer of the SSD1289.
      • So in this example: n = 1 + 16, so n^17 = 131072(round to 128KB) which makes sense.
      • However, Where are they getting this information? I can't find it listed anywhere in the reference manual. Is this the same for the K53?
  4. How do you set the system clock (or MCGOUTCLK)?
    • When Setting the Flexbus clock I understand that it has to be under 50MHz by design but also slower than my Clock cycle time on my display. In the case of my display it is 120ns, which means it has to be 32MHz or slower for it to write properly. I found that In order to get 32MHz, i need get the system clock at 96MHz and then set the following:
    • #define FLEX_CLK_INIT SIM_CLKDIV1_OUTDIV3(2)// FlexBus = Sysclk/3 pg314
      
      SIM->CLKDIV1 |= FLEX_CLK_INIT;‍‍‍‍‍‍‍‍‍‍‍‍
    • The problem is I'm sure exactly how to set MCGOUTCLK. I know i have to choose either the PLL or FLL and multiply an oscillator by a value but I'm a little lost on what registers i need to write to.
  5. For register FB_CSCR0[PS], What is the difference between between setting as 0x2 vs 0x3? They both seem to set 16-bit port sizes.
  6. Why does KDS force you to refrence registers via structure and not directly like below?
    • SIM_SOPT2 |= SIM_SOPT2_FBSL(3) 

Links:

Code:

#include <MK53D10.h>

void flexinit(void);
void vfnSendDataWord(unsigned short value);
void vfnSendCmdWord(unsigned short cmd);

#define ALT5 (PORT_PCR_MUX(5)|PORT_PCR_DSE_MASK) // Alternative function 5 = FB enable pg279
#define ALT1 (PORT_PCR_MUX(1)|PORT_PCR_DSE_MASK) // Alternative function 1 = GPIO pg279
#define FLEX_CLK_INIT SIM_CLKDIV1_OUTDIV3(3)// FlexBus = Sysclk/2 pg314
//#define FLEX_CLK_INIT (SIM_CLKDIV1 |=CLKDIV1 SIM_CLKDIV1_OUTDIV3(1))// FlexBus = Sysclk/2 pg314

void flexinit(void){
     //SIM_SCGC5 System clock gating control Register 5 pg.309
     //Enables clocks for all ports
     SIM->SCGC5 |= SIM_SCGC5_PORTA_MASK | SIM_SCGC5_PORTB_MASK | SIM_SCGC5_PORTC_MASK | SIM_SCGC5_PORTD_MASK | SIM_SCGC5_PORTE_MASK;
     SIM->CLKDIV1 |= FLEX_CLK_INIT;


/*     These are the K60 pinouts
 *      PORTC_PCR9=ALT5;
     PORTC_PCR10=ALT5;
     PORTC_PCR11=ALT5;
     PORTD_PCR1=ALT5;
     PORTD_PCR2=ALT5;
     PORTD_PCR3=ALT5;
     PORTD_PCR4=ALT5;
     PORTD_PCR5=ALT5;
     PORTD_PCR6=ALT5;
     PORTB_PCR17=ALT5;
     PORTB_PCR18=ALT5;
     PORTC_PCR0=ALT5;
     PORTC_PCR1=ALT5;
     PORTC_PCR2=ALT5;
     PORTC_PCR3=ALT5;
     PORTC_PCR4=ALT5;
     PORTC_PCR5=ALT5;
     PORTC_PCR6=ALT5;
     PORTC_PCR7=ALT5;
     PORTC_PCR8=ALT5; */

     //Change them to TWR-K53 Pinouts
     //Data Lines
     PORTA->PCR[10]=ALT5;     //EBI_AD15
     PORTA->PCR[24]=ALT5;     //EBI_AD14
     PORTA->PCR[25]=ALT5;     //EBI_AD13
     PORTA->PCR[26]=ALT5;     //EBI_AD12
     PORTA->PCR[27]=ALT5;     //EBI_AD11
     PORTA->PCR[28]=ALT5;     //EBI_AD10
     PORTD->PCR[10]=ALT5;     //EBI_AD9
     PORTD->PCR[11]=ALT5;     //EBI_AD8
     PORTD->PCR[12]=ALT5;     //EBI_AD7
     PORTD->PCR[13]=ALT5;     //EBI_AD6
     PORTD->PCR[14]=ALT5;     //EBI_AD5
     PORTE->PCR[8]=ALT5;          //EBI_AD4
     PORTE->PCR[9]=ALT5;          //EBI_AD3
     PORTE->PCR[10]=ALT5;     //EBI_AD2
     PORTE->PCR[11]=ALT5;     //EBI_AD1
     PORTE->PCR[12]=ALT5;     //EBI_AD0
     //Control Lines
     PORTA->PCR[6]=ALT5;          //CLKOUT0
     PORTD->PCR[15]=ALT5;     //EBI_R/W
     PORTE->PCR[7]=ALT5;          //EBI_CS0_B
     PORTA->PCR[9]=ALT5;          //EBI_AD16
     //Reset pin not on FB
     PORTD->PCR[4]=ALT1;          //Set as GPIO
     GPIOD->PDDR = 0x10;          //Set as output

     //SIM_SOPT2 is the System Options Register 2 Pg 292
     //Flexbus security level set to 11; off-chip instruction accesses and data accesses are allowed
     SIM->SOPT2 |= SIM_SOPT2_FBSL(3);
     //SIM_SCGC7 is the System clock gating control register 7 pg313
     //Sets the Flexbus clock to enabled
     SIM->SCGC7 |= SIM_SCGC7_FLEXBUS_MASK;

     #define FLEX_DC_ADDRESS      0x60000000
     #define FLEX_BASE_ADDRESS      0x60010000
     #define FLEX_ADRESS_MASK      0x00010000
     FB->CS[0].CSAR = FLEX_DC_ADDRESS; // CS0 base address

     #define FLEX_CSMR_V_MASK FB_CSMR_V_MASK               //0x1U
     FB->CS[0].CSMR = FLEX_ADRESS_MASK | FB_CSMR_V_MASK; // The address range is set to 128K because the DC signal is connected on address wire

     // MUX mode + Wait States
     #define FLEX_CSCR_MUX_MASK (FB_CSCR_BLS_MASK)      //Sets the BLS to right-aligned (0x200U)
     #define FLEX_CSCR_AA_MASK FB_CSCR_AA_MASK          //Sets the AA to Enable           (0x100U)
     #define FLEX_CSCR_PS1_MASK (FB_CSCR_PS(2))          //Sets the Port Size to 16bit     (0x080U)  //(((uint32_t)(((uint32_t)(x)) << FB_CSCR_PS_SHIFT)) & FB_CSCR_PS_MASK)
     FB->CS[0].CSCR = FLEX_CSCR_MUX_MASK | FLEX_CSCR_AA_MASK | FLEX_CSCR_PS1_MASK; // FlexBus setup as fast as possible in multiplexed mode
}

void vfnSendDataWord(unsigned short value)
 {
 *((unsigned short*)FLEX_BASE_ADDRESS) = value;
 }

void vfnSendCmdWord(unsigned short cmd)
{
*((unsigned short*)FLEX_DC_ADDRESS) = cmd;
}


int main(void) {
  /* Init board hardware. */
  //BOARD_InitPins();
  //BOARD_BootClockRUN();
  //BOARD_InitDebugConsole();
  flexinit();

  for(;;) { /* Infinite loop to avoid leaving the main function */
       //Check to see if each individual bit is working
       vfnSendCmdWord(0x0000);
       vfnSendDataWord(0x0001);
       vfnSendDataWord(0x0002);
       vfnSendDataWord(0x0004);
       vfnSendDataWord(0x0008);
       vfnSendDataWord(0x0010);
       vfnSendDataWord(0x0020);
       vfnSendDataWord(0x0040);
       vfnSendDataWord(0x0080);
       vfnSendDataWord(0x0100);
       vfnSendDataWord(0x0200);
       vfnSendDataWord(0x0400);
       vfnSendDataWord(0x0800);
       vfnSendDataWord(0x1000);
       vfnSendDataWord(0x2000);
       vfnSendDataWord(0x4000);
       vfnSendDataWord(0x8000);
    __asm("NOP"); /* something to use as a breakpoint stop while looping */
  }
}‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Thanks for any help and time,

Paul

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

5,637件の閲覧回数
mjbcswitzerland
Specialist V

Hi Paul

This is the K53 TFT configuration in the uTasker project:

    #define GLCD_COMMAND_ADDR         0x60400000
    #define GLCD_DATA_ADDR            0x60410000
                                      _CONFIG_PERIPHERAL(A, 9,  (PA_9_FB_AD16  | PORT_DSE_HIGH | PORT_PS_DOWN_ENABLE));
                                      _CONFIG_PERIPHERAL(A, 10, (PA_10_FB_AD15 | PORT_DSE_HIGH | PORT_PS_DOWN_ENABLE));
                                      _CONFIG_PERIPHERAL(A, 24, (PA_24_FB_AD14 | PORT_DSE_HIGH | PORT_PS_DOWN_ENABLE));
                                      _CONFIG_PERIPHERAL(A, 25, (PA_25_FB_AD13 | PORT_DSE_HIGH | PORT_PS_DOWN_ENABLE));
                                      _CONFIG_PERIPHERAL(A, 26, (PA_26_FB_AD12 | PORT_DSE_HIGH | PORT_PS_DOWN_ENABLE));
                                      _CONFIG_PERIPHERAL(A, 27, (PA_27_FB_AD11 | PORT_DSE_HIGH | PORT_PS_DOWN_ENABLE));
                                      _CONFIG_PERIPHERAL(A, 28, (PA_28_FB_AD10 | PORT_DSE_HIGH | PORT_PS_DOWN_ENABLE));
                                      _CONFIG_PERIPHERAL(D, 10, (PD_10_FB_AD9  | PORT_DSE_HIGH | PORT_PS_DOWN_ENABLE));
                                      _CONFIG_PERIPHERAL(D, 11, (PD_11_FB_AD8  | PORT_DSE_HIGH | PORT_PS_DOWN_ENABLE));
                                      _CONFIG_PERIPHERAL(D, 12, (PD_12_FB_AD7  | PORT_DSE_HIGH | PORT_PS_DOWN_ENABLE));
                                      _CONFIG_PERIPHERAL(D, 13, (PD_13_FB_AD6  | PORT_DSE_HIGH | PORT_PS_DOWN_ENABLE));
                                      _CONFIG_PERIPHERAL(D, 14, (PD_14_FB_AD5  | PORT_DSE_HIGH | PORT_PS_DOWN_ENABLE));
                                      _CONFIG_PERIPHERAL(E, 8,  (PE_8_FB_AD4   | PORT_DSE_HIGH | PORT_PS_DOWN_ENABLE));
                                      _CONFIG_PERIPHERAL(E, 9,  (PE_9_FB_AD3   | PORT_DSE_HIGH | PORT_PS_DOWN_ENABLE));
                                      _CONFIG_PERIPHERAL(E, 10, (PE_10_FB_AD2  | PORT_DSE_HIGH | PORT_PS_DOWN_ENABLE));
                                      _CONFIG_PERIPHERAL(E, 11, (PE_11_FB_AD1  | PORT_DSE_HIGH | PORT_PS_DOWN_ENABLE));
                                      _CONFIG_PERIPHERAL(E, 12, (PE_12_FB_AD0  | PORT_DSE_HIGH | PORT_PS_DOWN_ENABLE));
                                      _CONFIG_PERIPHERAL(E, 7,  (PE_7_FB_CS0   | PORT_DSE_HIGH | PORT_PS_DOWN_ENABLE));
                                      _CONFIG_PERIPHERAL(D, 15, (PD_15_FB_RW   | PORT_DSE_HIGH | PORT_PS_DOWN_ENABLE));
                                      CSAR0  = GLCD_COMMAND_ADDR; \
                                     CSMR0  = (0x00010000 | FB_CS_VALID); \
                                     CSCR0  = (FB_BLS | FB_AA | PORT_SIZE_16);‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍


I didn't spot any differences.

- Note that CSCR0 PS value of 2 is the 16 bit setting. A setting of 3 may work but such a setting is not defined as a valid one and so should be avoided.
- Block size is set by 0x00010000 in SMSR0 - matching the command/address setting where FB_AD16 is then used as command/data selection.
- The FlexBus clock is derived from the core clock divided by the value in CLKDIV1 (DIV3) as you have shown - see the uTasker simulator output below which emulates the K53 and a TFT and also displays the clock values that the code is setting. Its pin emulator displays the selected MUX values so that this can be checked (example of hovering the mouse over the PTD10 (the FB_AD9 function)

Regards

Mark

pastedImage_1.png

uTasker GLCD library with Kinetis and Display simulation: http://www.utasker.com/docs/uTasker/uTaskerLCD.PDF
Videos: https://youtu.be/AdtRyQ-2IrE / https://youtu.be/2Rbz1SOoJVI


uTasker developer and supporter (+5'000 hours experience on +60 Kinetis derivatives in +80 product developments)
Kinetis: http://www.utasker.com/kinetis.html

0 件の賞賛
返信

5,637件の閲覧回数
psantos
Contributor I

Hi Mark,

Thanks for the quick response. I've started looking into uTasker and it looks like it will be really helpful.

I think I found out why all my lines recently went haywire. I currently have a TWR-K53N512 board attached to the TWR-ELV modules and my TFT display attached to the Primary Elevator via 2mm to 2.54mm jumper cables. I recently decided to do a continuity check to make sure some data lines weren't touching and found that lines A80-73 on the Primary elevator were connected somehow. I began probing around more and started disconnecting my entire setup. It seems that with the power on and nothing connected but the K53 and the Elevator modules, A80-73 is connected and my 5V bus is showing continuity with ground and so is my 3.3v bus(Not great). I moved further up to just have only the K53 and I checked if PE11 and PE12 were connected somewhere on the board. This lead me to check pin 2,3 and 6 on the J2 header but found that these were not showing continuity at all.

So right now i'm at a loss of what parts may be possibly broken. The board seems like it still programs/debugs fine. Do you have any suggestions on what points to probe to tell if my K53 or my Elevator modules are dead?

Thanks again,

Paul

0 件の賞賛
返信

5,637件の閲覧回数
mjbcswitzerland
Specialist V

Hi Paul

I have a few tower kits and one of them had a back-plane/elevator with a break in a bus connection (internally) which I needed to correct by soldering a wire in parallel to.

As with all HW there can be a fault but I don't have a suggestion as to where to actually check.

The best thing to do is use a logic analyser to check the complete bus timing since you will then immediately see if something is stuck (due to short circuit, open circuit or setup error).
If you don't have this possibility I would load code that toggles all of the signals that are to be used (in GPIO mode) so that you can check that each one is arriving at its destination using a single scope channel (and if the voltage swing is not good it will also be seen). It is best if you can individually turn then on and off as desired so that you can be sure that you are measuring the one of interest and not one shorted to another line, etc.

Good luck

Regards

Mark

0 件の賞賛
返信

5,637件の閲覧回数
psantos
Contributor I

Hi Mark,

Sorry about the later response and thanks for your suggestions.

I've actually had some time recently to poke at my TWR-K53 board and I've notice a few things.

  1. I have loaded essentially a blank project to the board and I still get continuity between FB_AD[0] -> FB_AD8(Pins 80-73 on the Primary Elevator).
  2. After this I figured I should find a way to test this without the TWR-ELV in the mix so I took them off and I started probing points directly on the board with the power still on.
    1. I first wanted to test if the 5v and 3v3 supplies were good. I used TP2 for the 5v, TP11 for the GND and TP7 for the 3v3 check. They all seems to register at correct supply values. So that seems good at least.
    2. Next i moved onto the Flexbus lines. I tested the lines directly at the Flexbus Address Latch(U1 in the image below). It turns out that if I probe the LATCH_FB[0] to LATCH_FB[7] , they are all connected but the MCU side of the latch is totally fine.
    3. Does this mean that my address latch is probably blown and I need to replace it? I looked into the data sheet and I can't find a situation where all of the outputs would be connected. Suggestions?TWR-K53 Latch.png

Thank you again for your time and help,

Paul

0 件の賞賛
返信

5,637件の閲覧回数
mjbcswitzerland
Specialist V

Hi Paul

if the lines are shorted together there must be something wrong.

You don't need the latch in your circuit so you could just remove it and connect the inputs to the outputs if you are certain that there is a problem with the chip.

Regards

Mark

0 件の賞賛
返信