Help!! FTM2_C0V does not update.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help!! FTM2_C0V does not update.

5,420件の閲覧回数
josegardo
Contributor I

Hello,

I am using the FTM2 in Output Compare mode. This timers get the reference clock through external clock (100 KHz), so it overflows each 655.4ms. I am interested in using the Channel Match interrupt capabilities of this peripheral, but the content of FTM2_C0V is never updated. The reference manual said that this register is updated in the next count of FTM2 after FTM2_C0V was written (in my case, CLKS !=0 and FTMEN=0) but it always remains the same value. Check this simple code:

PE_ISR(FTM2_overflow)

{

  FTM2_C0SC &= (uint32_t)~0x80UL; //Clear flag

  sendUart(FTM2_C0V);                     //Print FTM2_C0V value

}

void setTimer(void)

{

  FTM2_C0V=0x7FFF;

  FTM2_C0SC &= (uint32_t)~0x80UL;    //Clear flag to clean previous channel matches

  FTM2_C0SC |= (uint32_t)0x40UL;        // Channel match interrupt enabled

}

When setTimer function is called, UART send the FTM2_C0V value each 655.4 ms, but this value is always 0x0000 (the default value) instead 0x7FFF.

Thank you

Jose

タグ(4)
0 件の賞賛
返信
12 返答(返信)

5,140件の閲覧回数
josegardo
Contributor I

We have not found out the solution :smileysad:. Anyone can help me?

0 件の賞賛
返信

5,140件の閲覧回数
Wlodek_D_
Senior Contributor II

Dear Jose Garcia Doblado,

Thank you for your post, however please consider moving it to the right community place for better visibility.

For details please see general advice https://community.freescale.com/docs/DOC-99909

Thank you for using Freescale Community.

Regards,

Wlodek_D.

0 件の賞賛
返信

5,140件の閲覧回数
Robinwithu
Senior Contributor I

Hi,

can you tell me which controller you are using?

Thanks and Regards,

Robin

0 件の賞賛
返信

5,140件の閲覧回数
josegardo
Contributor I

I am using a Kinetis K30 microcontroller, the MK30DN512ZVLQ10.

Thanks,

Jose

0 件の賞賛
返信

5,140件の閲覧回数
Robinwithu
Senior Contributor I

Like

void setTimer(void)

{

FTM2_MOD=0xFFFF;

  FTM2_C0V=0x7FFF;

  FTM2_C0SC &= (uint32_t)~0x80UL;    //Clear flag to clean previous channel matches

  FTM2_C0SC |= (uint32_t)0x40UL;        // Channel match interrupt enabled

}

Thanks n Regards,

Robin

0 件の賞賛
返信

5,140件の閲覧回数
josegardo
Contributor I

I have tried it but It does not work.

I was able to update the FTM2_C0V value stopping the counter CLKS=00 and the restarting again. But this solution is not valid for me. FTM2 is the synchornization time in a CDMA system and it can not be stopped. This is the code:

{void setTimer(void)

  FTM2_SC &=(uint32_t)~0x18UL;

  FTM2_C0V=0x7FFF;

  FTM2_SC |=(uint32_t)0x18UL;

  FTM2_C0SC &= (uint32_t)~0x80UL;    //Clear flag to clean previous channel matches

  FTM2_C0SC |= (uint32_t)0x40UL;        // Channel match interrupt enabled

}

Any other solution?

Thanks,

Jose

0 件の賞賛
返信

5,140件の閲覧回数
Robinwithu
Senior Contributor I

Hi Jose,

give me sometime i will look into that.if you will get the solution please post it.

Thanks n Regards,

Robin

0 件の賞賛
返信

5,140件の閲覧回数
josegardo
Contributor I

Hi Robin,

I'll do that.

Thanks

Jose

0 件の賞賛
返信

5,140件の閲覧回数
Robinwithu
Senior Contributor I

Hi Jose,

so what was problem?

Thanks n Regards,

Robin

0 件の賞賛
返信

5,140件の閲覧回数
josegardo
Contributor I

Sorry, I mean that I'll post the solution if I resolve the problem.

Thanks

0 件の賞賛
返信

5,140件の閲覧回数
Robinwithu
Senior Contributor I

Hi Jose,

can you mail me your complete code so that i can simulate on my pc.?

my email           [email protected]

Thanks n Regards,

Robin

0 件の賞賛
返信

5,140件の閲覧回数
Robinwithu
Senior Contributor I

Hi Jose,

can you initilize your FTM_MOD  to 0xFFFF , register in first case and see the result.

Regards,

Robin

0 件の賞賛
返信