Help!! FTM2_C0V does not update.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help!! FTM2_C0V does not update.

5,644 Views
josegardo
Contributor I

Hello,

I am using the FTM2 in Output Compare mode. This timers get the reference clock through external clock (100 KHz), so it overflows each 655.4ms. I am interested in using the Channel Match interrupt capabilities of this peripheral, but the content of FTM2_C0V is never updated. The reference manual said that this register is updated in the next count of FTM2 after FTM2_C0V was written (in my case, CLKS !=0 and FTMEN=0) but it always remains the same value. Check this simple code:

PE_ISR(FTM2_overflow)

{

  FTM2_C0SC &= (uint32_t)~0x80UL; //Clear flag

  sendUart(FTM2_C0V);                     //Print FTM2_C0V value

}

void setTimer(void)

{

  FTM2_C0V=0x7FFF;

  FTM2_C0SC &= (uint32_t)~0x80UL;    //Clear flag to clean previous channel matches

  FTM2_C0SC |= (uint32_t)0x40UL;        // Channel match interrupt enabled

}

When setTimer function is called, UART send the FTM2_C0V value each 655.4 ms, but this value is always 0x0000 (the default value) instead 0x7FFF.

Thank you

Jose

Tags (4)
0 Kudos
Reply
12 Replies

5,364 Views
josegardo
Contributor I

We have not found out the solution :smileysad:. Anyone can help me?

0 Kudos
Reply

5,364 Views
Wlodek_D_
Senior Contributor II

Dear Jose Garcia Doblado,

Thank you for your post, however please consider moving it to the right community place for better visibility.

For details please see general advice https://community.freescale.com/docs/DOC-99909

Thank you for using Freescale Community.

Regards,

Wlodek_D.

0 Kudos
Reply

5,364 Views
Robinwithu
Senior Contributor I

Hi,

can you tell me which controller you are using?

Thanks and Regards,

Robin

0 Kudos
Reply

5,364 Views
josegardo
Contributor I

I am using a Kinetis K30 microcontroller, the MK30DN512ZVLQ10.

Thanks,

Jose

0 Kudos
Reply

5,364 Views
Robinwithu
Senior Contributor I

Like

void setTimer(void)

{

FTM2_MOD=0xFFFF;

  FTM2_C0V=0x7FFF;

  FTM2_C0SC &= (uint32_t)~0x80UL;    //Clear flag to clean previous channel matches

  FTM2_C0SC |= (uint32_t)0x40UL;        // Channel match interrupt enabled

}

Thanks n Regards,

Robin

0 Kudos
Reply

5,364 Views
josegardo
Contributor I

I have tried it but It does not work.

I was able to update the FTM2_C0V value stopping the counter CLKS=00 and the restarting again. But this solution is not valid for me. FTM2 is the synchornization time in a CDMA system and it can not be stopped. This is the code:

{void setTimer(void)

  FTM2_SC &=(uint32_t)~0x18UL;

  FTM2_C0V=0x7FFF;

  FTM2_SC |=(uint32_t)0x18UL;

  FTM2_C0SC &= (uint32_t)~0x80UL;    //Clear flag to clean previous channel matches

  FTM2_C0SC |= (uint32_t)0x40UL;        // Channel match interrupt enabled

}

Any other solution?

Thanks,

Jose

0 Kudos
Reply

5,364 Views
Robinwithu
Senior Contributor I

Hi Jose,

give me sometime i will look into that.if you will get the solution please post it.

Thanks n Regards,

Robin

0 Kudos
Reply

5,364 Views
josegardo
Contributor I

Hi Robin,

I'll do that.

Thanks

Jose

0 Kudos
Reply

5,364 Views
Robinwithu
Senior Contributor I

Hi Jose,

so what was problem?

Thanks n Regards,

Robin

0 Kudos
Reply

5,364 Views
josegardo
Contributor I

Sorry, I mean that I'll post the solution if I resolve the problem.

Thanks

0 Kudos
Reply

5,364 Views
Robinwithu
Senior Contributor I

Hi Jose,

can you mail me your complete code so that i can simulate on my pc.?

my email           [email protected]

Thanks n Regards,

Robin

0 Kudos
Reply

5,364 Views
Robinwithu
Senior Contributor I

Hi Jose,

can you initilize your FTM_MOD  to 0xFFFF , register in first case and see the result.

Regards,

Robin

0 Kudos
Reply