Hello, is possible use Li-SOCl2 battery with open circuit voltage 3,68V to direct power MKL16Z128VFT4? It is only 80 mV over maximum voltage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hello, is possible use Li-SOCl2 battery with open circuit voltage 3,68V to direct power MKL16Z128VFT4? It is only 80 mV over maximum voltage

1,374 Views
tomasnez
Contributor I

We have low power device powered with pimary battery and we would like avoid to use voltage regulator because it has own consumption. Selected battery has over 3,6V (around 3,68V at 20°C in open circuit). What MCU for these conditions? Is it OK to use?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,189 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Tomas,

   From the MKL16Z128VF4 datasheet, we can get that the max data of VDD is 3.6 V.

   So we highly recommend the customer use the VDD is in the range of 1.71 to 3.6v, if the voltage is higher, it may cause the chip damaged.

   But from my own experience about the lithium battery, the open circuit voltage normally is higher than the closed circuit voltage, if you add the load, the battery voltage may lower than 3.6V. You can try to add your batter to the MKL16, and then test the vdd, whether it is in the range of 1.71 to 3.6V, if yes, you can use it.

Wish it helps you!

Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply