Having a problem when write data into on chip flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Having a problem when write data into on chip flash

2,099件の閲覧回数
jqy
Contributor I

I tried to modify the demo code" frdmkl03z_driver_examples_flash_pflash".  i coped the code from the main() to my code. It works fine to initialize the driver, read the data and even erase the sector. The problem is when it programmed the data in to the flash sector, a hard fault event happened. Any idea about this problem? 

i couldn't run the demo code on my own development board.

0 件の賞賛
返信
3 返答(返信)

1,977件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

See http://www.utasker.com/kinetis/FRDM-KL03Z.html
At the bottom of that page there is a binary that you can try and also a link to a video explaining the operation. All code, including a number of different parameter system options, is available in the uTasker project (allows also simulation of the KL03 and its internal Flash operation).

 

Regards

 

Mark

0 件の賞賛
返信

1,977件の閲覧回数
jqy
Contributor I

Hi Mark,

Thank you for your help! 

The code is working now. The problem is not form this part of code.

Jieqiu

0 件の賞賛
返信

1,977件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Jieqiu Yang,

    Thank you for your updated information!

    If your question is solved, please mark the correct answer to close this question.

    Thank you and have a nice day!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信