Hello Jonathan,
(For example the KE06 )
- Which IDE do you use , could you show all the code of the FTM0 initialization ?
- The FTM0/FTM1 with basic TPM functions , the FTM2 module with full functions , also the available registers are different .
(You can refer to the Reference manual pg82)
- If you use KDS or CW , you can use the PE to configure it , then you can see the generate code like this :

Hope it helps
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Have a great day,
Alice