HEXIWEAR FLEXCAN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HEXIWEAR FLEXCAN

1,281 Views
nagaswaroop_hc
Contributor I

HI NXP Team,

I am trying to implement  FlexCAN bus in Hexiwear i am not able to get the example code of that.

Please send the FlexCAN code for TX and RX.

Thanks & Regards

Swaroop

Engineer-Embedded Software

0 Kudos
Reply
1 Reply

1,167 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi NAGASWAROOP HC,

    As I know, the HEXIWEAR is using the MK64FN1M0VDC12 chip, this chip have the flexCAN module, so you can use the CAN function.

    You can download the K64 SDK code, the link is:

https://mcuxpresso.nxp.com/en/select 

  Select the K64 chip, then generate the code and download it.

  After you download it, you can find the flexCAN code in folder:

SDK_2.2_TWR-K64F120M\boards\twrk64f120m\driver_examples\flexcan

Wish it helps you!

If you still have question about it, please kindly let me know.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply