I am a bit confused.
Before I watched the video,
1. I build the project for Flash target.
2. I started the debugger by pressing "F11", then pressed the "play" button which loaded the code. It is working as it is supposed to.
3. When I disconnect and repower the device, The program is not running? as I didnt see any LED blinking.
After watching the video,
1. Does uTasker work as some sort of bootloader?
2. Is it possible to program it with any extra code in the sameway we do in uVision? (As in uVision, the flashed image is loaded even after the power cycle)
Thanks for helping.