Getting Started guide for FRDM-KW40Z IAR gives error message Fatal error: CPU did not power up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Getting Started guide for FRDM-KW40Z IAR gives error message Fatal error: CPU did not power up

2,397 Views
tjoncas
Contributor I

When following the Getting Started guide for FRDM-KW40Z (NXP Freedom Development Platform for Kinetis |NXP ), upon reaching step 3 "build and run", using ANY of the sample projects, during the step to download and debug (see http://cache.nxp.com/files/32bit/doc/user_guide/MKW40ZSMACSW303QSG.pdf ), I get a message box that says "Fatal error: CPU did not power up. Session aborted."  I notice in the debugger log that the last line before an error is always "Loading the CMSIS-DAP driver ".  Both boards definitely work with the pre-programmed sample program so I don't think they came dead on arrival.  Does anyone have any advice?

2 Replies

1,754 Views
tjoncas
Contributor I

For reference, here is a sample Debug Log:

Tue Feb 09, 2016 15:57:26: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.3\arm\config\debugger\Freescale\KLxx.dmac

Tue Feb 09, 2016 15:57:27: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.3\arm\config\flashloader\Freescale\FlashKW01.mac

Tue Feb 09, 2016 15:57:27: Loading the CMSIS-DAP driver

Tue Feb 09, 2016 15:57:27: Probe: CMSIS-DAP probe SW module ver 1.11

Tue Feb 09, 2016 15:57:27: Probe: CMSIS-DAP S/N '0290ff039ED54E0F9E29B367' mapped to a number 00367.

Tue Feb 09, 2016 15:57:27: EARM v.3.96

Tue Feb 09, 2016 15:57:27: Emulation layer version 3.96

Tue Feb 09, 2016 15:57:27: Notification to core-connect hookup.

Tue Feb 09, 2016 15:57:27: MDM-AP detected

Tue Feb 09, 2016 15:57:27: Probe: ConnectSpec='MBED CMSIS-DAP:0290ff039ED54E0F9E29B367:8-317CFB24-0-0000'.

Tue Feb 09, 2016 15:57:28: Connecting to TAP#0 DAP AHB-AP-CM port 0 (IDR=0x4770031).

Tue Feb 09, 2016 15:57:28: Recognized CPUID=0x410cc601 Cortex-M0+ r0p1 arch ARMv6-M

Tue Feb 09, 2016 15:57:28: Debug resources: 2 instruction comparators, 2 data watchpoints.

Tue Feb 09, 2016 15:57:28: CPU status OK

Tue Feb 09, 2016 15:57:28: LowLevelReset(hardware, delay 200)

Tue Feb 09, 2016 15:57:28: CPU status FAILED

Tue Feb 09, 2016 15:57:28: CMD_INTERPRETER: failed

Tue Feb 09, 2016 15:57:28: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.3\arm\config\debugger\Freescale\KLxx.dmac(82,17): Error: Operation error.

Tue Feb 09, 2016 15:57:28: Error while calling macro execUserCoreConnect

Tue Feb 09, 2016 15:57:28: CMD_INTERPRETER: failed

Tue Feb 09, 2016 15:57:28: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.3\arm\config\debugger\Freescale\KLxx.dmac(82,17): Error: Operation error.

Tue Feb 09, 2016 15:57:28: Error while calling macro execUserCoreConnect

Tue Feb 09, 2016 15:57:28: CMD_INTERPRETER: failed

Tue Feb 09, 2016 15:57:28: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.3\arm\config\debugger\Freescale\KLxx.dmac(82,17): Error: Operation error.

Tue Feb 09, 2016 15:57:28: Error while calling macro execUserCoreConnect

Tue Feb 09, 2016 15:57:28: CMD_INTERPRETER: failed

Tue Feb 09, 2016 15:57:28: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.3\arm\config\debugger\Freescale\KLxx.dmac(82,17): Error: Operation error.

Tue Feb 09, 2016 15:57:28: Error while calling macro execUserCoreConnect

Tue Feb 09, 2016 15:57:28: CMD_INTERPRETER: failed

Tue Feb 09, 2016 15:57:28: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.3\arm\config\debugger\Freescale\KLxx.dmac(82,17): Error: Operation error.

Tue Feb 09, 2016 15:57:28: Error while calling macro execUserCoreConnect

Tue Feb 09, 2016 15:57:28: CMD_INTERPRETER: failed

Tue Feb 09, 2016 15:57:28: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.3\arm\config\debugger\Freescale\KLxx.dmac(82,17): Error: Operation error.

Tue Feb 09, 2016 15:57:28: Error while calling macro execUserCoreConnect

Tue Feb 09, 2016 15:57:28: CMD_INTERPRETER: failed

Tue Feb 09, 2016 15:57:28: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.3\arm\config\debugger\Freescale\KLxx.dmac(82,17): Error: Operation error.

Tue Feb 09, 2016 15:57:28: Error while calling macro execUserCoreConnect

Tue Feb 09, 2016 15:57:28: CMD_INTERPRETER: failed

Tue Feb 09, 2016 15:57:28: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.3\arm\config\debugger\Freescale\KLxx.dmac(82,17): Error: Operation error.

Tue Feb 09, 2016 15:57:28: Error while calling macro execUserCoreConnect

Tue Feb 09, 2016 16:02:52: Fatal error: CPU did not power up  Session aborted!

Tue Feb 09, 2016 16:02:52: Unloaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.3\arm\config\flashloader\Freescale\FlashKW01.mac

Tue Feb 09, 2016 16:02:53: Logging to file: C:\Freescale\KW40Z_Connectivity_Software_1.0.1\ConnSw\examples\ieee_802_15_4\MyWirelessApp\Coordinator\frdmkw40z\FreeRTOS\build\iar\cspycomm.log

Tue Feb 09, 2016 16:02:53: Loading the CMSIS-DAP driver

1,754 Views
franciscomezana
NXP Employee
NXP Employee

Hi Tom,

I recommend to take a look to this previous threat.

Fatel error:cpu did not power up session aborted!

It shows the resolution for the same problem with another customer.

I hope this information helps.

0 Kudos
Reply