Getting Error in the Startup.C file provided by Freescale For TWR-K20D5 module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Getting Error in the Startup.C file provided by Freescale For TWR-K20D5 module

3,366件の閲覧回数
Amit_Kumar1
Senior Contributor II

hello

 

I am using KEIL MDK , I added startup.c file I got the following error on building the project.

 

startup.c(234): error:  #18: expected a ")"

 

I have attached the files kindly check it. These 2 files were present in

 

kinetis_50MHz_sc\k20d50m_sc_pex\common\Kinetis\startup  folder which I downloaded from

 

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-K20D50M&fpsp=1&tab=Design_Tools_T...

 

Thanks in advance

Original Attachment has been moved to: startup.c.zip

Original Attachment has been moved to: startup_ARM_CC.c.zip

ラベル(3)
タグ(4)
5 返答(返信)

2,870件の閲覧回数
perlam_i_au
Senior Contributor I

I already checked those files and as you can see they are part of the folder named "common", all of those files should be used as part of the project (since they are associated to each other); in the folder named "projects" you can find tree different example projects, only "helloword" has examples for both: IAR  and CodeWarrior. Everything else inside those folders are for CodeWarrior only.

2,871件の閲覧回数
Amit_Kumar1
Senior Contributor II

Hi Perla

Thanks for the reply.  In common folder, there are 133 files how would I know which file is essential to use for my Project as I am trying to make a project based on UART1. I think there should be a separate file which is a base file used for all the projects that I think is this startup.c file. 

Regards,

Amit Kumar

0 件の賞賛
返信

2,871件の閲覧回数
Monica
Senior Contributor III

Hello Amit,

was this suggestion useful?

Please keep us posted, we'd like to know :smileywink:

Best,

Monica.

0 件の賞賛
返信

2,871件の閲覧回数
Amit_Kumar1
Senior Contributor II

Hi Monica

The above solution didn't worked. And due to the poor support and lack of document for KEIL uvision4 MDK. I switched to codewarrior with processorexpert.

Regards

Amit Kumar

0 件の賞賛
返信

2,871件の閲覧回数
perlam_i_au
Senior Contributor I

I suggest you create your project folder in the code exmaples directory [k20d50m_sc_pex/projects/], for this specific case "helloworld", if you create it in this folder you will not have to worry about which files from the common folder the compiler will have to use.

0 件の賞賛
返信