GUI development tool for Kinetis MUC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GUI development tool for Kinetis MUC

1,944件の閲覧回数
nelsonlobo
Contributor II

Hi,

Was looking for solutions on GUI development using 4.3" TFT screen 40pin parallel connection. Found eGUI available on Freescale website.

Im planning to use the MK02FN64VLH10  MCU. Would the libraries support this MUC. If not then is there any RAD tool for developing screens and buttons using the same ???

Regards,

Nelson Lobo

ラベル(1)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,606件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Nelson,

Kinetis MCU is supported by the Freescale eGUI and you can find more information through the link as below.

Freescale eGUI: Graphical LCD Driver for MCUs|Freescale
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,606件の閲覧回数
LuisCasado
NXP Employee
NXP Employee
0 件の賞賛
返信