GPIO Pin's State on power-up

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GPIO Pin's State on power-up

7,661 次查看
eduardrazumovsk
Contributor III

Hello,

I'm designing a system with K64 MCU

My question regarding all GPIO's state on power-up :

1. The GPIO's state on boot is output or input ? if so, is it PU/PD/HiZ ?

2. What doe's it mean that the default function of a GPIOs is "DISABLED" ?

Looking at the reference manual - http://cache.freescale.com/files/microcontrollers/doc/ref_manual/K64P144M120SF5RM.pdf

Page 244, chapter 10.2.2 Port control and interrupt summary

"Pull enable at reset - Disabled" - so i can understand from that that the GPIO is defined as Input Hi-Z ?

Please clarify this issue for me

Thanks & Regards

0 项奖励
回复
3 回复数

5,479 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Eduard Razumovsky:

Mark's response is completely correct. You should look at the Default column in the pinout table.

DISABLED indicates no function after reset, so that is High-Impedance.

Pins with an analog MUX option will be connected by default after reset to their corresponding analog module.

Regards!

Jorge Gonzalez

5,479 次查看
gschelotto
Contributor V

Okay, but what about this case on my MK02Z?

powering up issue on MKE02Z GPIO

On power-up PTB4 seems to follow the VCC ramp and after PE initialization this is set as a digital output with zero value.

regards,

gaston

0 项奖励
回复

5,479 次查看
mjbcswitzerland
Specialist V

Hi

No pins are GPIOs outputs after reset.

If their pull-up is disabled at reset it means that there is no pull-up or pull-down connected. [Only the pins that default to JTAg use have pull-ups or downs eabled out of reset].

Some pins default to peripheral functions (see 10.3.1) and not GPIO.

If disabled out of reset, it means that there is no connected default function - the pin is not GPIO input without first setting the GPIO Mux function (Alt 1).

Regards

Mark

Kinetis: µTasker Kinetis support

K64: µTasker Kinetis FRDM-K64F support  / µTasker Kinetis TWR-K64F120M support  / µTasker Kinetis TWR-K65F180M support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 项奖励
回复