GPCLR_WR does not work???

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

GPCLR_WR does not work???

跳至解决方案
2,939 次查看
pietrodicastri
Senior Contributor II

Good morning.

I am trying to use the  HW_PORT_GPCLR_WR without success.

In this stub of code the kGpioEncMux2 kGpioEncMux1 kGpioEncMux0 are the bit 9 8 7 of the PORTC.

The GPIO_HAL_WritePinOutput  works, but if I try to use the HW_PORT_GPCLR_WR it does not...

The bit of the register appear to be correct, but the output is different.

Suggestions???

typedef union _mux_bits_t

{

  struct

  {

       uint32_t sp : 7;

       uint32_t mux : 3;

       uint32_t sp2 : 22;

  };

  struct

  {

       uint32_t sp3 : 23;

       uint32_t muxact : 3;

       uint32_t sp4 : 6;

  };

  uint32_t val;

} avago_mux_bits_t;

avago_mux_bits_t mux_bits = { 0 };

void inline static avago_mux_out( uint8_t muxval )

{

  muxval ^= 0xFF; // just negate for the ULN open collector

  mux_bits.mux = muxval;

  mux_bits.muxact = 7;

  HW_PORT_GPCLR_WR( g_portBaseAddr[ GPIO_EXTRACT_PORT(kGpioEncMux2) ], mux_bits.val );

  GPIO_HAL_WritePinOutput( g_gpioBaseAddr[ GPIO_EXTRACT_PORT( kGpioEncMux2 ) ], GPIO_EXTRACT_PIN( kGpioEncMux2 ), muxval & 4 );

  GPIO_HAL_WritePinOutput( g_gpioBaseAddr[ GPIO_EXTRACT_PORT( kGpioEncMux1 ) ], GPIO_EXTRACT_PIN( kGpioEncMux1 ), muxval & 2 );

  GPIO_HAL_WritePinOutput( g_gpioBaseAddr[ GPIO_EXTRACT_PORT( kGpioEncMux0 ) ], GPIO_EXTRACT_PIN( kGpioEncMux0 ), muxval & 1 );

}

标签 (1)
标记 (1)
1 解答
2,794 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Pietro,

    I check your code which you past,

  HW_PORT_GPCLR_WR( g_portBaseAddr[ GPIO_EXTRACT_PORT(kGpioEncMux2) ], mux_bits.val );

  This is not correct, because HW_PORT_GPCLR_WR definition is like following in our KSDK:

#define HW_PORT_GPCLR_ADDR(x)((uint32_t)(x) + 0x80U)

#define HW_PORT_GPCLR(x)  (*(__O hw_port_gpclr_t *) HW_PORT_GPCLR_ADDR(x))
#define HW_PORT_GPCLR_RD(x)(HW_PORT_GPCLR(x).U)

#define HW_PORT_GPCLR_WR(x, v)  (HW_PORT_GPCLR(x).U = (v))

x: is the base address of PORTC, it is  0x4004_B000. then x+0x80 =0x4004_B080

2.jpg

So, you should configure it like this :

  HW_PORT_GPCLR_WR(PORTC_BASE,0X03800103 );

This will configure the PORTC_PCR7, PORTC_PCR8 and PORTC_PCR9.

I test it, it can works ok on my side with HW_PORT_GPCLR_WR(PORTC_BASE,0X03800103 );

Following are my test result:

(1)Before run :HW_PORT_GPCLR_WR(PORTC_BASE,0X03800103 );


3.jpg

(2) After run ::HW_PORT_GPCLR_WR(PORTC_BASE,0X03800103 );

4.jpg

So, please modify your code and test again.

Any question, please contact me!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

5 回复数
2,794 次查看
pietrodicastri
Senior Contributor II

I appreciate the effort. I am not able to make it work. I need to give up for now I can live with normal writing.

Thank You

0 项奖励
回复
2,795 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Pietro,

    I check your code which you past,

  HW_PORT_GPCLR_WR( g_portBaseAddr[ GPIO_EXTRACT_PORT(kGpioEncMux2) ], mux_bits.val );

  This is not correct, because HW_PORT_GPCLR_WR definition is like following in our KSDK:

#define HW_PORT_GPCLR_ADDR(x)((uint32_t)(x) + 0x80U)

#define HW_PORT_GPCLR(x)  (*(__O hw_port_gpclr_t *) HW_PORT_GPCLR_ADDR(x))
#define HW_PORT_GPCLR_RD(x)(HW_PORT_GPCLR(x).U)

#define HW_PORT_GPCLR_WR(x, v)  (HW_PORT_GPCLR(x).U = (v))

x: is the base address of PORTC, it is  0x4004_B000. then x+0x80 =0x4004_B080

2.jpg

So, you should configure it like this :

  HW_PORT_GPCLR_WR(PORTC_BASE,0X03800103 );

This will configure the PORTC_PCR7, PORTC_PCR8 and PORTC_PCR9.

I test it, it can works ok on my side with HW_PORT_GPCLR_WR(PORTC_BASE,0X03800103 );

Following are my test result:

(1)Before run :HW_PORT_GPCLR_WR(PORTC_BASE,0X03800103 );


3.jpg

(2) After run ::HW_PORT_GPCLR_WR(PORTC_BASE,0X03800103 );

4.jpg

So, please modify your code and test again.

Any question, please contact me!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,794 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Pietro,

    Could you tell me the full name of your chp and where  you get the code.

    You can control the PORTx_GPCLR and PORTx_GPCHR register directly,  this will work fine.

   Waiting for your reply!

Jingjing

0 项奖励
回复
2,794 次查看
pietrodicastri
Senior Contributor II

Hei Jingjing

Thank You for follow up.

I am using the FRDM K64.

I hope You can solve the arcan.

Thank You

0 项奖励
回复
2,794 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Pietro,

GPCLR is define the bits[15:0] of PORTx_PCRn, it includes pin mux control , pull select, pull enable,etc.

Did you configure your PTC7,PTC8,PTC9 as GPIO(MUX = 1), please check the according register:PORTC_PCR7,PORTC_PCR8,PORTC_PCT9.

Besides, check your GPIOC_PDDR, GPIOC_PDOR, whether you configure it as the output, and the pin out voltage is correct or not.

please give me your register debug picture, and your testing project.

Regards.

Jingjing

0 项奖励
回复