From Shell Linux - Loading new software in MK66F and relaunch (restart)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

From Shell Linux - Loading new software in MK66F and relaunch (restart)

1,801 次查看
daniel_mouren
Contributor II

Hi,

I'm using the K66F FRDM and I want to load new binary software using the linux shell.

These steps already succeed:

  1. Generate a binary file.
  2. Copy this file to the boot loader
  3. Unplug and plug in the USB cable

11-usb-opensda.PNG

But here is the manual access to the USB cable is not possible and I have to find a way with the Linux shell to reboot the card.

note: I also opened a ticket on the stack exchange community.

Linux Shell / Power off USB port

Thank you in advance

标记 (3)
0 项奖励
回复
1 回复

1,684 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please check here to download latest OpenSDA firmware for FRDM-K66F board.

I tested to download Segger J-Link firmware from here and after updated the firmware, I could drag and drop application image (*.bin) to MSD USB disk (FRDM-K66FJ).

pastedImage_1.png

About how to update FRDM-K66F on board OpenSDA firmware, please check below picture:

pastedImage_2.png

Wish it helps.


Have a great day,
Mike

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复