Freemaster tutorial for mkv10z16

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freemaster tutorial for mkv10z16

ソリューションへジャンプ
3,360件の閲覧回数
Frogram
Contributor I

Hi, all

I bought  a  MKV10Z16 for FOC control a robot in-wheel motor.

I have ST-LINK, so I tried to connect MKV10 and freemaster with that but failed.

I can't even connect or check whether its running,

any tutorial or example for starting freemaster?

Thanks.

0 件の賞賛
返信
1 解決策
3,353件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Frogram,

I didn't find the ST-LINK in the list of debugger probe of FreeMASTER Connection Wizard.

Connect through a debugger probe or on-board debugger interface.png

Try to identify the Backgroud Debug Module (BDM) probe you are using.png

I don’t know if ST-Link has a USB to UART function, if so, you can try to choose this connection method.

Use plain-old serial line or USB-to-Serial Converter cable.pngProbing UART Ports.png

We have a FreeMASTER community forum, I suggest you go there to ask questions and get more accurate answers.

You can find tutorial or example there:

  • Check out FreeMASTER How To article

FreeMASTER How To.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
3,354件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Frogram,

I didn't find the ST-LINK in the list of debugger probe of FreeMASTER Connection Wizard.

Connect through a debugger probe or on-board debugger interface.png

Try to identify the Backgroud Debug Module (BDM) probe you are using.png

I don’t know if ST-Link has a USB to UART function, if so, you can try to choose this connection method.

Use plain-old serial line or USB-to-Serial Converter cable.pngProbing UART Ports.png

We have a FreeMASTER community forum, I suggest you go there to ask questions and get more accurate answers.

You can find tutorial or example there:

  • Check out FreeMASTER How To article

FreeMASTER How To.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

3,343件の閲覧回数
Frogram
Contributor I

I am looking at, but it seems support only developer boards like frdm

how could I just start with standalone chip?

thanks

0 件の賞賛
返信
3,346件の閲覧回数
Frogram
Contributor I

Thanks!

I'll check and try them!

0 件の賞賛
返信