Freedom board - "Device is secure. Erase to unsecure?"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freedom board - "Device is secure. Erase to unsecure?"

ソリューションへジャンプ
13,900件の閲覧回数
mindthomas
Contributor I

Everytime we try to program, debug or erase our Freescale Freedom board using the OpenSDA JTAG interface we get this error inside CodeWarrior:

"Device is secure. Erase to unsecure?"

The board has been working fine before.

Then we used the "Flash Programmer" inside CodeWarrior to program one of the binary files (.bin) from the "kl25_sc" package (sample codes) and since that we haven't been able to program, debug or erase.

Has the device mistakenly been put into "Mass erase disable"-mode? If yes, howcome and why did this happen - CodeWarrior didn't even warn us!?

Regards Thomas

ラベル(1)
0 件の賞賛
返信
1 解決策
7,151件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

I have found a solution which works for me to unsecure the Freedom board again:

Unsecuring the KL25Z Freedom Board | MCU on Eclipse

I hope this works for others too.

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
17 返答(返信)
7,151件の閲覧回数
crezyoz
Contributor IV

I just began experiencing the exact same issue. I resolve it by setting the speed of the Multilink to 0.2 Mhz instead of 1Mhz.

Though I find it interesting because the prompt doesn't say what device is secure.

0 件の賞賛
返信
7,151件の閲覧回数
kevintai
Contributor I

My development environment FRDM-KL25Z and  KEIL

I can not find the setting of Multilink speed.

0000.jpg

0 件の賞賛
返信
7,151件の閲覧回数
BlackNight
NXP Employee
NXP Employee

It is that 'debug shift speed' in your screenshot.

Try adjusting that setting.

Hope this helps,

Erich

0 件の賞賛
返信
7,151件の閲覧回数
kevintai
Contributor I

I try all the speed, but the issue is still here.:smileyangry:

0 件の賞賛
返信
7,151件の閲覧回数
chris_brown
NXP Employee
NXP Employee

kevintai,

The KEIL debugger does not modify the flash configuration fields if the binary that you tried to program does not explicitly tell KEIL to modify these fields.  Consequently, if you have setup your environment to perform a mass erase, and then program the binary (which doesn't modify the flash configuration fields), then your part will be in a secured state with mass erase enabled.

To fix this, try setting KEIL to only perform sector erases and see if this helps.

Also, if you will provide us with the binary that you tried, we can fix the binary in our next sample code release so that a mass erase is possible without this frustration you are experiencing.

Thanks!

CB

0 件の賞賛
返信
7,151件の閲覧回数
gregkon
Contributor I

Hi

I have the same problem, I use MK10DX256VLK7, "multilink universal" and IAR environment. (also codewarrior is available).

I have no idea what happend. This build what I have flashed is used on other board without any problem. I have never touch any scecure bits.

1. Is any way what I may do in order to unsecure it?

2. is it possible that it is hardware problem with board (uC or connection)?

I have try adjusting debug speed as mentioned above but without any success.

Please advise if someone has any idea.

/Greg

0 件の賞賛
返信
7,151件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Greg,

see about secure/protecting the device: http://mcuoneclipse.com/2012/11/04/how-not-to-secure-my-microcontroller/

So I hope the 'mass erase disabled' bit is not set, otherwise the device is really locked.

Sometimes it is false alarm too, if the connection is not working properly, or wrong files are used, see Device is secure? | MCU on Eclipse

I hope this helps,

Erich

0 件の賞賛
返信
7,151件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Greg,

missed to mention that if you have a Segger J-Link, you load the Segger OpenSDA firmware on your FRDM board (but your device does not indicate that you are using a FRDM board)?

In any case: http://mcuoneclipse.com/2014/10/05/unlocking-and-erasing-flash-with-segger-j-link/

Erich

0 件の賞賛
返信
7,151件の閲覧回数
gregkon
Contributor I

Hi

Thank you for support.

I use custom board, only access by JTAG.

under address 0x40C i 0x31 and 0x40D is 0x30. So it looks ok for me, mass erase i enabled.

I do not have any other tool than multilink universal.

I wonder if it may be a hardware problem with connection to uC.

0 件の賞賛
返信
7,151件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Yes, I think it could be a hardware/connection problem. Because that 'secure' message comes up too if the microcontroller is not really accessible or does not respond. You might check the reset line and the other debug lines with an oscilloscope.

Erich

0 件の賞賛
返信
7,151件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Ok, just throwing in something here, and it is a wild guess.

I run into a clock setup issue for running the USB port. For this I had to use the external clock.

See

and Tutorial: USB CDC with the KL25Z Freedom Board | MCU on Eclipse and

Completing the FRDM-KL25Z Board | MCU on Eclipse

Are you using the external clock? If so, maybe the device is clocked so weird that the opeSDA has a problem to connect to the KL25Z.

It is at least worth a try: if your board has R25 not populated, add that 1 MOhm resistor to it. Maybe it makes a difference?

I really hope that helps.

If not: maybe send me the S19 file of the application you have programmed. I'll take the risk to burn one of my boards.

Erich

0 件の賞賛
返信
7,151件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

Thomas has sent me a binary file which indeed secures the device (that dialog pops up), but I can successfully recover and reflash the device. And I can do this with CodeWarrior and the OpenSDA (no Multilink needed).

I was able to do this with two black boards, one with R25 and the other without that resistor. It does not make a difference for me, at least with this file.

Here are is the information from my boards:

Board Name is: FRDM-KL25Z
MicroBoot Kernel Version is: 1.01
Bootloader Version is: 1.01
Installed Application: PEMicro Debug App
Application Version is: 1.02

Could you verify you have the same? You get that information if you plug-in the board in Bootloader mode and open the SDA_INFO.HTM from the MSD device (see OpenSDA on the Freedom KL25Z Board | MCU on Eclipse).


One thing to note: if your application disables the mass erase bit, then you cannot recover the board (as disabling the mass erase means really locking the microcontroller!!!!).


Hope this helps,

Erich


0 件の賞賛
返信
7,151件の閲覧回数
BlackNight
NXP Employee
NXP Employee

good news: I finally have received a binary file, and now I can reproduce it with my board. The good news is: It seems I have found a way how to get control back and perform a mass erase with CodeWarrior. I'll write up the steps and verify again that it works for me, and I can hopefully report back positive news very soon.

0 件の賞賛
返信
7,152件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

I have found a solution which works for me to unsecure the Freedom board again:

Unsecuring the KL25Z Freedom Board | MCU on Eclipse

I hope this works for others too.

Erich

0 件の賞賛
返信
7,151件の閲覧回数
kevintai
Contributor I

It is OK,TKS:smileyhappy:

0 件の賞賛
返信
7,151件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

which *.bin file have you used? In the kl25_sc these are all Keil and IAR projects, but they should not set the mass erase disable flag. 'Device is secure' is shown in case the OpenSDA is not able to get hold of the device. At least with OSBDM/OSJTAG I had cases where OSBDM/OSJTAG was not able to recover a device, showing that dialog. Using the P&E Universal Multilink (with a JTAG/BDM connector) I was able to recover the device.

Hope this helps,

Erich

7,150件の閲覧回数
kevintai
Contributor I

I have  the same issue.

But i have no the P&E Universal Multilink.

Any other  solution ?

0 件の賞賛
返信