Freedom Board for K10 Dev.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freedom Board for K10 Dev.

ソリューションへジャンプ
2,137件の閲覧回数
eduardoumana
Contributor III

I am doing some preliminary research in order to get started developing with the Kinetis K10_50 family of MCUs. It seems the development board to use would be the KWIKSTIK-K40. My question is, is it possible/advisable to use the Freedom dev. board instead? It seems to me the KWIKSTIK is an overkill for my particular application, and I also feel rather unfamiliar with its construction given it doesn't have any pins.

Thank you!

0 件の賞賛
返信
1 解決策
1,933件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Eduardo:

Actually the closest development board for your device is FRDM-K20D50M or TWR-K20D50M. First is the Freedom Board for K20/K10 50 Mhz devices and second is the Tower System version for the same families.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,934件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Eduardo:

Actually the closest development board for your device is FRDM-K20D50M or TWR-K20D50M. First is the Freedom Board for K20/K10 50 Mhz devices and second is the Tower System version for the same families.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,933件の閲覧回数
eduardoumana
Contributor III

I am glad to hear this. I had the idea this was the case, but there is no indication under "Evaluation/Development Boards and Systems" on the K10 - 50Mhz product page.

K10_50 |Kinetis K10 50 MHz MCUs|Freescale

0 件の賞賛
返信