FreeRTOS in the mke04z8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FreeRTOS in the mke04z8

ソリューションへジャンプ
788件の閲覧回数
carlesls
Contributor II

is it possible to add FreeRTOS to a mke04z8 microcontroller?

Usually in other boards there is a FreeRTOS template for it.

 

carlesls_0-1731925292325.png

I check the MKE17z and there is a template for FreeRTOS.

carlesls_1-1731925414973.png

 

 

 

 

ラベル(1)
0 件の賞賛
返信
1 解決策
752件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @carlesls ,

Thanks for your post. 

In versions earlier than SDK2.5.0, you can find FreeRTOS examples. Refer to the figure below.

Celeste_Liu_0-1732072033205.png

For example, SDK 2.4.1:

Celeste_Liu_1-1732072067341.png

Wish it helps. If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

Best Regard,

Celeste

元の投稿で解決策を見る

1 返信
753件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @carlesls ,

Thanks for your post. 

In versions earlier than SDK2.5.0, you can find FreeRTOS examples. Refer to the figure below.

Celeste_Liu_0-1732072033205.png

For example, SDK 2.4.1:

Celeste_Liu_1-1732072067341.png

Wish it helps. If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

Best Regard,

Celeste