Floating point on k6xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Floating point on k6xx

ソリューションへジャンプ
2,330件の閲覧回数
pietrodicastri
Senior Contributor II

Good morning

I need to optimize the floating point execution. The CPU is the K64...

I have been looking for similar thematics, but I did not find the right answer. I understand the core is offering the FPU only for the shorter floating,

while for the double only the software emulation is available.

I see the math.h is proposing the functions ex...

sin()  and sinf()

for the data of type float and double. In parallel the CMSYS has the function arm_sin_f32() not the arm_sin_f64()

So I have some limited trouble in evaluating the usage of the functions.

1) It seemd for double data type the only function to use is the sin()

2) If I use the sinf() the hardware support is automatically used???

3) Is the arm_sin_f32()  better than the sinf() ? Precision wise ???

I would like to be sure the FPU is used. What is the way to verify??? Maybe looking the disassembled code for some floating point instruction....

I will pleasantly book some advice on the subject

Thank You

ラベル(1)
タグ(1)
1 解決策
1,955件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Pietro,

I have used the following code based on KDS tools, the f2 return the correct result.

BR

XiangJun Rong

#include "MKV58F22.h"

#include "math.h"

#define PI 3.1415926

static int i = 0;

double f1,f2;

int main(void)

{

    /* Write your code here */

    f1=1.23;

    f2=1.23;

    f2=f1+f2;

    f1=PI/4.0;

    f2=sin(f1);

    __asm("nop");  //set break point here to observe the result in debugger

    /* This for loop should be replaced. By default this loop allows a single stepping. */

    for (;;) {

        i++;

    }

    /* Never leave main */

    return 0;

}

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,955件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Pietro,

As you said that the Kinetis family K64 has FPU module, which supports float operation. The Floating-Point Unit (FPU) provides IEEE754-compliant operations on single-precision, 32-bit, floating-point values. But the FPU does not support 64 bits double operation.

The CMSIS library only support arm_sin_f32(), arm_sin_q15() anf arm_sin_q31() data format sin operation, but the CMSIS does not support double data format operation either.

Regarding the double data format sin() function, of course, the compiler uses software simulation to implement the double data type sin() function. But it is dependent on the compiler tools whether the double data type sin(0 function is implemented or not.

which compiler tools are you using, KDS, codewarrior for mcu, IAR, Keil? you have to consult the compiler individually.

BR

Xiangjun Rong

1,956件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Pietro,

I have used the following code based on KDS tools, the f2 return the correct result.

BR

XiangJun Rong

#include "MKV58F22.h"

#include "math.h"

#define PI 3.1415926

static int i = 0;

double f1,f2;

int main(void)

{

    /* Write your code here */

    f1=1.23;

    f2=1.23;

    f2=f1+f2;

    f1=PI/4.0;

    f2=sin(f1);

    __asm("nop");  //set break point here to observe the result in debugger

    /* This for loop should be replaced. By default this loop allows a single stepping. */

    for (;;) {

        i++;

    }

    /* Never leave main */

    return 0;

}

0 件の賞賛
返信
1,955件の閲覧回数
pietrodicastri
Senior Contributor II

Hi xiangjun.rong

I am trying th get familiar with the FPU, with some help and some try and retry. Thank You  for the suggestions.

If You have time, have You tested if the arm_sin_f32() is better than the sinf() ???

Thank You

0 件の賞賛
返信
1,955件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Pie,

I think both the function can give correct result, but the arm_sin_f32() takes short time, but the sinf() takes long time due to the fact that the function is implemented by software simulation.

Hope it can help you.

BR

Xiangjun Rong

0 件の賞賛
返信