Flickering console in eGUI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flickering console in eGUI

ソリューションへジャンプ
2,859件の閲覧回数
Thommi_Tulpe
Contributor IV

Hello,

i am using a console on the LCD (TWR-LCD).

I am useng a TWR-K60N512 with TWR-LCD.

I am using a console in one screen. The screen is flickering. I think it is because the

D4D_Poll() Funktion witch redraws the screen periodictly.

(D4D_RedrawScreen(pScreen); in D4D_Poll)

 

Is it possibe to redraw the screen only when something is changed ?

This is when I put a character or string to the console or the flashing cursor.

 

Or is it possible only to redraw what is change and not the hole screen ?

 

Best Regards

Thommi

0 件の賞賛
返信
1 解決策
2,639件の閲覧回数
Thommi_Tulpe
Contributor IV

Problem solved

 

I changed the TWR-LCD and everything is O.K.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,640件の閲覧回数
Thommi_Tulpe
Contributor IV

Problem solved

 

I changed the TWR-LCD and everything is O.K.

0 件の賞賛
返信
2,639件の閲覧回数
iafg
Contributor IV

Do you mean you physically changed it?

We had a similar issue with the TWR-PIM-41WVGA, but it simply turned out that the regulator on the K70 was at it's limits.

http://futurefreescaleguy.wordpress.com/2012/05/04/future-twr-pim-41wvga-sample-project/#comment-18

OK when powered from the elevator...

 

 

0 件の賞賛
返信