Flexbus on K53 with MII/RMII network

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flexbus on K53 with MII/RMII network

ソリューションへジャンプ
2,937件の閲覧回数
kfranz
Contributor III

We need to use the flexbus on a K53 and maintain the ability to use RMII for the network interface. There seems to be a conflict with pin usage when trying to do this.

How do I use flexbus and still use the RMII interrface?

 

0 件の賞賛
返信
1 解決策
2,931件の閲覧回数
kfranz
Contributor III

My goal is to connect an external SRAM chip. Preferably with at least 128KB of SRAM.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,932件の閲覧回数
kfranz
Contributor III

My goal is to connect an external SRAM chip. Preferably with at least 128KB of SRAM.

0 件の賞賛
返信
2,759件の閲覧回数
kfranz
Contributor III

We accomplished this by not connecting the trace pins. PTA6 (TRACE_CLKOUT), PTA7 (TRACE_D3), PTA8 (TRACE_D2), PTA9 (TRACE_D1), and PTA10 (TRACE_D0) were originally connected to the Cortex-M JTAG 20-pin debugger. If you are not using the JTAG trace capability, these pins do not need to be connected to the debugger. They can then be used for the flexbus. This makes connecting an external RAM to the flexbus possible and also use the RMII interface. 

0 件の賞賛
返信