Flexbus on K53 with MII/RMII network

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flexbus on K53 with MII/RMII network

Jump to solution
2,063 Views
kfranz
Contributor III

We need to use the flexbus on a K53 and maintain the ability to use RMII for the network interface. There seems to be a conflict with pin usage when trying to do this.

How do I use flexbus and still use the RMII interrface?

 

0 Kudos
Reply
1 Solution
2,057 Views
kfranz
Contributor III

My goal is to connect an external SRAM chip. Preferably with at least 128KB of SRAM.

View solution in original post

0 Kudos
Reply
2 Replies
2,058 Views
kfranz
Contributor III

My goal is to connect an external SRAM chip. Preferably with at least 128KB of SRAM.

0 Kudos
Reply
1,885 Views
kfranz
Contributor III

We accomplished this by not connecting the trace pins. PTA6 (TRACE_CLKOUT), PTA7 (TRACE_D3), PTA8 (TRACE_D2), PTA9 (TRACE_D1), and PTA10 (TRACE_D0) were originally connected to the Cortex-M JTAG 20-pin debugger. If you are not using the JTAG trace capability, these pins do not need to be connected to the debugger. They can then be used for the flexbus. This makes connecting an external RAM to the flexbus possible and also use the RMII interface. 

0 Kudos
Reply