Flexbus decryption support for code execution

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flexbus decryption support for code execution

ソリューションへジャンプ
2,777件の閲覧回数
bbenj
Contributor III

Hello,

Does FlexBus supports (seamless) decryption for code execution on external flash?

Especially for the K6x series. I read that code execution from flexbus is possible, but can it be encrypted?

Thank you,

Best Regards,

Benjamin

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
2,663件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Kinetis Flexbus doesn't has seamless decryption for code execution on external flash.

Customer could select i.MX RT series product, such as RT1060 which support this feature.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,664件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Kinetis Flexbus doesn't has seamless decryption for code execution on external flash.

Customer could select i.MX RT series product, such as RT1060 which support this feature.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,663件の閲覧回数
bbenj
Contributor III

Hi,

Thank you, the i.MX RT series seems to fit our needs. One thing I couldn't find definitive answer for though: can I use JTAG to download and debug code to/from the external flash on FlexSPI/QSPI (which supports on-the-fly decryption)?

Is there any reference document on FlexSPI/QSPI usage with encryption?

Also, does any of the LPC series have external flash with encryption support (with code execution, etc)?

Thank you,

Best Regards,

Benjamin

0 件の賞賛
返信
2,663件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Benjiamin,

Please post a new question thread at i.MX product sub-community about FlexSPI/QSPI security application. Thanks for understanding.

I know LPC5500 has this feature with internal Flash.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,663件の閲覧回数
bbenj
Contributor III

Ok, thank you!

Have a nice day,

Benjamin

0 件の賞賛
返信