Flexbus decryption support for code execution

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flexbus decryption support for code execution

Jump to solution
2,974 Views
bbenj
Contributor III

Hello,

Does FlexBus supports (seamless) decryption for code execution on external flash?

Especially for the K6x series. I read that code execution from flexbus is possible, but can it be encrypted?

Thank you,

Best Regards,

Benjamin

Labels (1)
0 Kudos
Reply
1 Solution
2,860 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Kinetis Flexbus doesn't has seamless decryption for code execution on external flash.

Customer could select i.MX RT series product, such as RT1060 which support this feature.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
2,860 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Kinetis Flexbus doesn't has seamless decryption for code execution on external flash.

Customer could select i.MX RT series product, such as RT1060 which support this feature.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,860 Views
bbenj
Contributor III

Hi,

Thank you, the i.MX RT series seems to fit our needs. One thing I couldn't find definitive answer for though: can I use JTAG to download and debug code to/from the external flash on FlexSPI/QSPI (which supports on-the-fly decryption)?

Is there any reference document on FlexSPI/QSPI usage with encryption?

Also, does any of the LPC series have external flash with encryption support (with code execution, etc)?

Thank you,

Best Regards,

Benjamin

0 Kudos
Reply
2,860 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Benjiamin,

Please post a new question thread at i.MX product sub-community about FlexSPI/QSPI security application. Thanks for understanding.

I know LPC5500 has this feature with internal Flash.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,860 Views
bbenj
Contributor III

Ok, thank you!

Have a nice day,

Benjamin

0 Kudos
Reply