Hi.
I am working with K61 MCU and MR2A16ACYS35 SRAM (4M size) through Flex Bus. I can write to and read from MRAM.
The problem: when I write to address 0x60000000 any data, the same data I view at addresses 0x60080000, 0x60100000. The same situation occurred when I write to one from these addresses (0x60080000 or 0x60100000) - the data updated in every 512K part at addresses: 0x60000000, 0x60080000, 0x60100000.
Why occurred write duplication? How can I correct this?
Thanks.
My configuration is:
// HW initialisation
#define MRAM_START_ADDRESS(*(volatile unsigned char*)(0x60000000))
FB_CSAR0 = (unsigned int)&MRAM_START_ADDRESS; //Set Base address
FB_CSCR0 = FB_CSCR_PS(1) // 8-bit port
| FB_CSCR_AA_MASK // auto-acknowledge
| FB_CSCR_WS(0x2) // 2 wait states
FB_CSMR0 = FB_CSMR_BAM(0x3F) // Set base address mask for 4M address space - up to 0x60400000
| FB_CSMR_V_MASK; // Enable cs valid signal
// Enable the clock to the FlexBus
SIM_SCGC7 |= SIM_SCGC7_FLEXBUS_MASK;
// FlexBus Clock not divided
SIM_CLKDIV1 |= SIM_CLKDIV1_OUTDIV3(0x0);
// Set the GPIO ports clocks
SIM_SCGC5 = SIM_SCGC5_PORTA_MASK | SIM_SCGC5_PORTB_MASK | SIM_SCGC5_PORTC_MASK |
SIM_SCGC5_PORTD_MASK | SIM_SCGC5_PORTE_MASK;
PORTB_PCR11 = PORT_PCR_MUX(5); // fb_ad[18]
PORTB_PCR16 = PORT_PCR_MUX(5); // fb_ad[17]
PORTB_PCR17 = PORT_PCR_MUX(5); // fb_ad[16]
PORTB_PCR18 = PORT_PCR_MUX(5); // fb_ad[15]
PORTC_PCR0 = PORT_PCR_MUX(5); // fb_ad[14]
PORTC_PCR1 = PORT_PCR_MUX(5); // fb_ad[13]
PORTC_PCR2 = PORT_PCR_MUX(5); // fb_ad[12]
PORTC_PCR4 = PORT_PCR_MUX(5); // fb_ad[11]
PORTC_PCR5 = PORT_PCR_MUX(5); // fb_ad[10]
PORTC_PCR6 = PORT_PCR_MUX(5); // fb_ad[9]
PORTC_PCR7 = PORT_PCR_MUX(5); // fb_ad[8]
PORTC_PCR8 = PORT_PCR_MUX(5); // fb_ad[7]
PORTC_PCR9 = PORT_PCR_MUX(5); // fb_ad[6]
PORTC_PCR10 = PORT_PCR_MUX(5); // fb_ad[5]
PORTD_PCR2 = PORT_PCR_MUX(5); // fb_ad[4]
PORTD_PCR3 = PORT_PCR_MUX(5); // fb_ad[3]
PORTD_PCR4 = PORT_PCR_MUX(5); // fb_ad[2]
PORTD_PCR5 = PORT_PCR_MUX(5); // fb_ad[1]
PORTD_PCR6 = PORT_PCR_MUX(5); // fb_ad[0]
PORTB_PCR20 = PORT_PCR_MUX(5); // fb_ad[31] used as d[7]
PORTB_PCR21 = PORT_PCR_MUX(5); // fb_ad[30] used as d[6]
PORTB_PCR22 = PORT_PCR_MUX(5); // fb_ad[29] used as d[5]
PORTB_PCR23 = PORT_PCR_MUX(5); // fb_ad[28] used as d[4]
PORTC_PCR12 = PORT_PCR_MUX(5); // fb_ad[27] used as d[3]
PORTC_PCR13 = PORT_PCR_MUX(5); // fb_ad[26] used as d[2]
PORTC_PCR14 = PORT_PCR_MUX(5); // fb_ad[25] used as d[1]
PORTC_PCR15 = PORT_PCR_MUX(5); // fb_ad[24] used as d[0]
PORTB_PCR19 = PORT_PCR_MUX(5); // fb_oe_b
PORTC_PCR11 = PORT_PCR_MUX(5); // fb_rw_b
PORTD_PCR1 = PORT_PCR_MUX(5); // fb_cs0_b
PORTD_PCR0 = PORT_PCR_MUX(5); // fb_ale
For read and write test:
uint8 wdata8 = 0x5A; // data to write to mram
uint8 rdata8; // variable to read mram
for(n=0x00000;n<0x000F;n++) // address offset
{
*(vuint8*)(&MRAM_START_ADDRESS + n) = wdata8;
rdata8 = 0x00; // clear data variable
rdata8 = (*(vuint8*)(&MRAM_START_ADDRESS + n));
}