FlexRAM not writable during Flash erase (FTFE_FCNFG->RAMRDY becomes 0)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FlexRAM not writable during Flash erase (FTFE_FCNFG->RAMRDY becomes 0)

1,608件の閲覧回数
noperator
Contributor I

Hello,

I would like to use FlexRAM on K24FN1M0V as general purpose RAM, but I noticed that after initiating a Flash mass erase, attempting to write to the FlexRAM leads to a hard fault. After the mass erase is finished, the RAM is accessible again, but it is erased to 0xFF.

I found in K24P144M120SF5RM Section 29.4.10.9:

The EEERDY and RAMRDY bits are clear during the Read 1s All Blocks operation and
are restored at the end of the Read 1s All Blocks operation

Is the same true for the 'Erase All Blocks' command? It is not documented.

Is there any way to prevent this so that FlexRAM can be used as general purpose RAM?

Thanks,

Ivan

0 件の賞賛
返信
2 返答(返信)

1,584件の閲覧回数
jay_heng
NXP Employee
NXP Employee

From RM: The Erase All Blocks operation erases all flash memory, initializes the FlexRAM, verifies all memory contents, and releases MCU security.

so it is the same true for the 'Erase All Blocks' command.

FlexRAM is part of FTF flash controller, it will always be effected by FTF operation.

0 件の賞賛
返信

1,581件の閲覧回数
noperator
Contributor I

Thanks for the confirmation, Jay. It would have been nice if the FTF left this RAM alone except for the 'Program Section' operation, but I understand it's a hardware limitation. I will stick to using the main RAM only.

0 件の賞賛
返信