Flex NVM K40

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flex NVM K40

1,559件の閲覧回数
Mar_adelos_ngel
Contributor I

Hi,

Does anyone know how to use flash memory emulate EEPROM?

Im using the K40 target.

Could you provide sample code tutorial?

 

Thank you

ラベル(1)
1 返信

1,205件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Maria:

You may check the application note AN4282, which instructs you on how to use the EEPROM functionality.

Also, if you installed CodeWarrior, there is an example code for the K40 in the next installation path:

C:\Freescale\CW MCU v10.6\MCU\CodeWarrior_Examples\Kinetis_Examples\k40\flexmem

I hope these references are useful.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------