Flex NVM K40

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flex NVM K40

1,600 Views
Mar_adelos_ngel
Contributor I

Hi,

Does anyone know how to use flash memory emulate EEPROM?

Im using the K40 target.

Could you provide sample code tutorial?

 

Thank you

Labels (1)
1 Reply

1,246 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Maria:

You may check the application note AN4282, which instructs you on how to use the EEPROM functionality.

Also, if you installed CodeWarrior, there is an example code for the K40 in the next installation path:

C:\Freescale\CW MCU v10.6\MCU\CodeWarrior_Examples\Kinetis_Examples\k40\flexmem

I hope these references are useful.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------