Flash programming MKE04Z64VLD4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash programming MKE04Z64VLD4

871 Views
owiaky
Contributor I

I am trying to repair a piece of equipment that one of these chips has failed. I was able to use Segger EDU Mini and J-Flash to read the fw from a known good chip but it does not let me write/flash to the new chip without a more expensive device or license. 

I am asking if there is some alternative that doesn't cost a ton of money to read/write to these chips. (MKE04Z64VLD4)

Thanks

0 Kudos
Reply
1 Reply

829 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @owiaky ,

Thanks for your post.

I recommend you use the mcu-link. It can be used with the KE04, and it only costs 13.99 USD.

MCU Link JTAG/SWD Debug Probe | NXP Semiconductors

 

Hope it can help you.

BRs,

Celeste

 

----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply