Flash programming MKE04Z64VLD4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flash programming MKE04Z64VLD4

1,021 次查看
owiaky
Contributor I

I am trying to repair a piece of equipment that one of these chips has failed. I was able to use Segger EDU Mini and J-Flash to read the fw from a known good chip but it does not let me write/flash to the new chip without a more expensive device or license. 

I am asking if there is some alternative that doesn't cost a ton of money to read/write to these chips. (MKE04Z64VLD4)

Thanks

0 项奖励
回复
1 回复

979 次查看
Celeste_Liu
NXP Employee
NXP Employee

Hello @owiaky ,

Thanks for your post.

I recommend you use the mcu-link. It can be used with the KE04, and it only costs 13.99 USD.

MCU Link JTAG/SWD Debug Probe | NXP Semiconductors

 

Hope it can help you.

BRs,

Celeste

 

----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复