Flash code for blhost

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash code for blhost

2,016件の閲覧回数
arunkannan
Contributor III

Is there a code for flashing using blhost

Please provide the same.

0 件の賞賛
返信
3 返答(返信)

2,000件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Can you tell us the part number of Kinetis family so that we can know if it supports blhost tools?

BR

XiangJun Rong

0 件の賞賛
返信

1,991件の閲覧回数
arunkannan
Contributor III

MKL16Z128VLH4, MKV10Z128VLF7, MKL16Z128VFT4 are the MCUs we are using

0 件の賞賛
返信

1,978件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls refer to the release note of blhost tools.

https://www.nxp.com.cn/docs/en/release-note/BLHOSTRN.pdf

Obviously, the KV10 support blhost tools with  Pre-programmed Flashloader.

But the KL16 does not supports blhost. But you can download the flashloader to internal RAM of KL16, then use blhost tools to download application code to on-chip flash of KL family.

This is flashloader link:

https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools...

 

Hope it cab help you

BR

XiangJun Rong

0 件の賞賛
返信