Flash code for blhost

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash code for blhost

1,992 Views
arunkannan
Contributor III

Is there a code for flashing using blhost

Please provide the same.

0 Kudos
Reply
3 Replies

1,976 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Can you tell us the part number of Kinetis family so that we can know if it supports blhost tools?

BR

XiangJun Rong

0 Kudos
Reply

1,967 Views
arunkannan
Contributor III

MKL16Z128VLH4, MKV10Z128VLF7, MKL16Z128VFT4 are the MCUs we are using

0 Kudos
Reply

1,954 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls refer to the release note of blhost tools.

https://www.nxp.com.cn/docs/en/release-note/BLHOSTRN.pdf

Obviously, the KV10 support blhost tools with  Pre-programmed Flashloader.

But the KL16 does not supports blhost. But you can download the flashloader to internal RAM of KL16, then use blhost tools to download application code to on-chip flash of KL family.

This is flashloader link:

https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools...

 

Hope it cab help you

BR

XiangJun Rong

0 Kudos
Reply