Firmware update of K65 MCU running MQX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Firmware update of K65 MCU running MQX

1,659 Views
annamol
Contributor IV

Hi,

I am planning to do firmware update on K65 MCU running MQX. While searching I came across

  • Kinetis boot loader v2 based on KDS
  • USB DFU boot loader
  • Flash swapping
  • MSD boot loader
  • USB host and device boot loader

I would love to try serial boot loader implementation based on KBOOT. Is there any example project available for MQX? Or is it only based on KDS?

Labels (2)
0 Kudos
Reply
2 Replies

1,442 Views
miduo
NXP Employee
NXP Employee

Hi,

No, we do not have the boot loader based on MQX, and you are correct, that we provide the MQX with the KSDK1.3.

0 Kudos
Reply

1,442 Views
annamol
Contributor IV

Hi,

For firmware update using KBOOT, is openSDA a must?

0 Kudos
Reply