Firmware update of K65 MCU running MQX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Firmware update of K65 MCU running MQX

1,697件の閲覧回数
annamol
Contributor IV

Hi,

I am planning to do firmware update on K65 MCU running MQX. While searching I came across

  • Kinetis boot loader v2 based on KDS
  • USB DFU boot loader
  • Flash swapping
  • MSD boot loader
  • USB host and device boot loader

I would love to try serial boot loader implementation based on KBOOT. Is there any example project available for MQX? Or is it only based on KDS?

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,480件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

No, we do not have the boot loader based on MQX, and you are correct, that we provide the MQX with the KSDK1.3.

0 件の賞賛
返信

1,480件の閲覧回数
annamol
Contributor IV

Hi,

For firmware update using KBOOT, is openSDA a must?

0 件の賞賛
返信