Firmware update of K65 MCU running MQX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Firmware update of K65 MCU running MQX

1,642 次查看
annamol
Contributor IV

Hi,

I am planning to do firmware update on K65 MCU running MQX. While searching I came across

  • Kinetis boot loader v2 based on KDS
  • USB DFU boot loader
  • Flash swapping
  • MSD boot loader
  • USB host and device boot loader

I would love to try serial boot loader implementation based on KBOOT. Is there any example project available for MQX? Or is it only based on KDS?

标签 (2)
0 项奖励
回复
2 回复数

1,425 次查看
miduo
NXP Employee
NXP Employee

Hi,

No, we do not have the boot loader based on MQX, and you are correct, that we provide the MQX with the KSDK1.3.

0 项奖励
回复

1,425 次查看
annamol
Contributor IV

Hi,

For firmware update using KBOOT, is openSDA a must?

0 项奖励
回复