Firmware placement for EzPort

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Firmware placement for EzPort

1,177 Views
alexeyusoltsev
Contributor IV

 Good day ladies and gentlemen,

I need help.

I've made project and a PCB (№2) that have to program main PCB(№1) through EzPort. For that purpose I am to make a firmware that contain firmware for itself and firmware for another board linked at curtain address(for board №1). 

 So my question is how can I link existing *elf file into project to place it in the flash under known address?(for further upload to another board through EzPort)

P.S.: I've heard that some utilities can convert *elf/*bin to .c files that i can deal with. But I'd glad to learn other solution to the problem.

 Best regards,

Alexey.

Tags (3)
0 Kudos
Reply
2 Replies

1,074 Views
mjbcswitzerland
Specialist V

Hi Alexey

You can use GCC "objcopy" to generate binary files from your elf files. Then you can use the uTasker utilities to combine them or to convert them to c files: http://www.utasker.com/forum/index.php?topic=1445.0
Tools and details at the link.

Also see the uTasker EzPort cloner that allows one board to clone another via EzPort:
http://www.utasker.com/docs/uTasker/uTaskerEzPortCloner.pdf

Regards

Mark


Kinetis: http://www.utasker.com/kinetis.html
Faster and cheaper project development....

1,074 Views
alexeyusoltsev
Contributor IV

 Hi Mark,

thanks for your interest and contribution!! I'll try to start with that.

 Best regards,

Alexey.

0 Kudos
Reply