Firmware MK70

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Firmware MK70

2,403件の閲覧回数
Microfelix
Contributor IV

Hello,
I ask if it is possible on a K70 processor, you can use the firmware via an external FLASH.
The Indoor 1 Mbyte space is almost finished. If I need more space as I do?

Maurizio Felicioni

2 返答(返信)

2,290件の閲覧回数
mjbcswitzerland
Specialist V

Hi

If your external Flash is parallel and memory mapped on the FlexBus it can be used for program code.

Often external SDRAM is also used (faster) to run code from, after copying it there for a cheaper serial Flash, or NAND flash device.

Regards

Mark

2,290件の閲覧回数
Microfelix
Contributor IV

hi,

I am using TWR K70 with external ddr2 ram.
I could put my firmware in a serial flash, and then copy it into RAM?
Is there any example?


Thank you very much

Maurizio

0 件の賞賛
返信