Firmware MK70

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Firmware MK70

2,386 Views
Microfelix
Contributor IV

Hello,
I ask if it is possible on a K70 processor, you can use the firmware via an external FLASH.
The Indoor 1 Mbyte space is almost finished. If I need more space as I do?

Maurizio Felicioni

2 Replies

2,273 Views
mjbcswitzerland
Specialist V

Hi

If your external Flash is parallel and memory mapped on the FlexBus it can be used for program code.

Often external SDRAM is also used (faster) to run code from, after copying it there for a cheaper serial Flash, or NAND flash device.

Regards

Mark

2,273 Views
Microfelix
Contributor IV

hi,

I am using TWR K70 with external ddr2 ram.
I could put my firmware in a serial flash, and then copy it into RAM?
Is there any example?


Thank you very much

Maurizio

0 Kudos
Reply