FatFS middleware Missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FatFS middleware Missing

ソリューションへジャンプ
4,571件の閲覧回数
songja
Contributor III

Hi,

I am trying to add FatFS driver but I couldn't find it when I was creating a new project thru SDK wizard.

I actually added all the available drivers and everything else on SDK wizard too but still there wasn't FatFS.

However, there is still a SDK example that is using FatFS.

(I made sure that OpenSDK for K66F includes FatFS middleware too. )

Everything.PNGpastedImage_2.png

does anybody know where I can add it?

Thanks.

ラベル(3)
タグ(3)
0 件の賞賛
返信
1 解決策
4,316件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi  JAEYONG

Fatfs is under the middleware components tab, not under drivers. Please see picture below

pastedImage_1.png

Regards

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
4,316件の閲覧回数
tomasvavra
Contributor I

This issue is still present in SDK 2.6.0.

0 件の賞賛
返信
4,316件の閲覧回数
tomasvavra
Contributor I

I have this problem too with LPCXpresso54618. My stack v2.5 is build with FatFs. I can see FatFs files inside the manifest xml file a import working FatFs example. But when I am cerating new project - FatFs is not listed in the middleware at all.

0 件の賞賛
返信
4,317件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi  JAEYONG

Fatfs is under the middleware components tab, not under drivers. Please see picture below

pastedImage_1.png

Regards

Daniel

0 件の賞賛
返信
4,316件の閲覧回数
songja
Contributor III

Hello, Daniel.

Under middleware tap, I can only see "Network" and "Security".

SDK wiz.png

Do I need to include other middleware when I build SDK? I remember 3 middlewares were included as default and I added freeRTOS on the top of them.

Thanks. 

Regards,
Jaeyong

0 件の賞賛
返信
4,316件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Yes, you need to make sure fatfs component is selected when you build SDK.

Regards

Daniel

0 件の賞賛
返信